Skip to main content
QSiji
Visitor II
December 12, 2018
Question

How to solve the problem? STM32CubeMX 5.0.0 These IPs still have some not configure or wrong parameter values:[FATFS]

The project was create in CubeMX of earlier verson 4.29.0 , and it can easily to generate code. But a couple of days earlier, I need to add a new pin to the project. So I added the pin configure in CubeMx of Verson 5.0.0. When I generate codes, tips above happens. So how to solve the problem.

This topic has been closed for replies.

1 reply

hwen
Visitor II
March 21, 2019

Set an input pin and select that input pin.