Skip to main content
Associate III
March 13, 2026
Question

How to Set Up the Full CUBEMX on the STM32N6570-DK Board

안녕하세요 STM32N6570-DK의 사용하기 위한 cubemx 설정이 필요합니다. 카메라, lcd, sd카드, usb, eth 등 기능을 다 살린 cubemx 설정 또는 ioc 파일을 받고 싶습니다. 확인 부탁 드립니다.

 

Hello, I need a cubemx setting for use of STM32N6570-DK. I would like to receive a cubemx setting or an ioc file that utilizes all the functions such as camera, lcd, sd card, usb, eth, etc. Please check it.

4 replies

MGogr.1
Senior
March 13, 2026

While creating new project you can directly select your Eval board with all its peripheral initialize.

LeeJaewonAuthor
Associate III
March 13, 2026

If you select a dk board from cubemx, it loses a few features and doesn't do the exact action.

TDK
March 13, 2026

What features does it lose?

"If you feel a post has answered your question, please click ""Accept as Solution""."