Associate II
Jun 24, 2021 12:08 PM UTC
Solved
How to run CubeMX-generated LWIP with LAN8742? DHCP doesn't work, but ST'example works.
- 3 replies
- 5691 views
Hello, I am trying to run a project generated by STM32cubeMX. DHCP thread code I got from ST example called "STM32H723 webserver demo" and put it to my code. Communication between PHY and STM32 works well, DHCP doesn't work. Even if I put a static IP, it doesn't connect to my router. But if I download that ST webserver example, everything is ok, and DHCP works. Where is the problem? I did Lwip configuration via CubeMX equal to Lwip configuration in that ST example, everything other is the same (linker areas, MPU config, etc). I haven't in my project an HTTP server yet, I just want to ping my device from my PC. DHCP stops at SELECTING state.