Skip to main content
PeterL
Associate III
Jan 27, 2022 3:34 PM UTC
Question

How to make a keil driver library out of HAL source. Weak definitions gets selected unexpectedly.

When doing generating a project from STM32CubeMX (for F4 family) and converting it to a library in keil, then when keeping main in executable project and linking to library wrong implementation of *MspInit gets selected. The weak ones are selected even though there is a "strong" one in library too.

Problem is how compilers work. They don't look extensively in librarys so they don't even bother to find the strong one if first stumbled upon a weak symbol.

 i.HAL_UART_Init 0x08001260 Section 0 stm32f4xx_hal_uart.o(i.HAL_UART_Init)
 i.HAL_UART_MspInit 0x080012c2 Section 0 stm32f4xx_hal_uart.o(i.HAL_UART_MspInit)

See keil map file above. The weak MspInit were selected despite the "strong" version is in library too.

For IAR there is an linker option --whole_archive that forces linker to actually look in all object files and then the strong one is selected.

For Keil I haven't fond similar option (neither old or clang based version).

This topic has been closed for replies.

1 reply

Pavel A.
Jan 28, 2022 5:13 AM UTC