Skip to main content
Ajudi.1
Associate
Jul 22, 2020 9:35 PM UTC
Question

How to import CMSIS DSP library without using CubeMX?

Hello everyone.

I'm trying to use some functions available in the CMSIS DSP Library.

First I tried to add the library through CubeMX->Additional Software, but found a known bug reported here. According to this link, this bug should be fixed for the next cubeMX release, due for this week.

Since I really can't wait for this bug to be fixed, I tried to manually copy use the source and header files provided in the Firmware package for my MCU (STM32F4 in this case).

Therefore, I was wondering if someone faced this problem and was able to succeed at adding these libraries without cubeMX

Best Regards

This topic has been closed for replies.

3 replies

Khouloud OTHMAN
Associate
Jul 23, 2020 3:40 PM UTC

Hello Ajudi.1,

The newly published pack ARM.CMSIS.5.7.0 is not compatible with CubeMX v5.6.1 and this will be fixed in the next version that will be available by the beginning of next week (sorry for delay). There is no problem with older CMSIS DSP versions (5.6.0 for example), you can import it using CubeMX.

BR,

Khouloud.

Ajudi.1
Ajudi.1Author
Associate
Jul 23, 2020 4:08 PM UTC

I'll Try using version 5.6.0, thank you!

Tesla DeLorean
Guru
Jul 23, 2020 4:17 PM UTC

>>Therefore, I was wondering if someone faced this problem and was able to succeed at adding these libraries without cubeMX

Sure, they are just source and include files, with perhaps a command line define.

I've built entire DSP library without even looking at CubeMX

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..