Skip to main content
kaushikbm
Associate II
February 19, 2023
Solved

How to generate a error free code with FreeRTOS for STM32G030 with STM32CubeMX for MDK-ARM

  • February 19, 2023
  • 3 replies
  • 5576 views

I'm using the latest 6.7.0 version of STM32CubeMX for generating the code. I'm selecting just the serial wire and the a different timer for tick generation and nothing else. The code generation is completed without any errors.

But when I try to compile I get about a zillion errors regarding FreeRTOS. Did a lot of search and tried different solutions provided. Like this one here. But nothing worked so far. :weary_face:

Has anybody tried similar config ?

Thanks in advance for your help :smiling_face_with_smiling_eyes:

Here is the starting and ending lines of the build output. Had to snip off a bit as the post was getting too long. :grinning_face_with_sweat:

Build started: Project: Test
*** Using Compiler 'V6.19', folder: 'C:\Keil_v5\ARM\ARMCLANG\Bin'
Build target 'Test'
compiling stm32g0xx_ll_rcc.c...
compiling stm32g0xx_hal_timebase_tim.c...
compiling app_freertos.c...
compiling main.c...
assembling startup_stm32g030xx.s...
compiling stm32g0xx_it.c...
compiling stm32g0xx_hal_msp.c...
compiling gpio.c...
compiling stm32g0xx_hal_rcc_ex.c...
compiling stm32g0xx_hal_flash.c...
compiling stm32g0xx_hal_rcc.c...
compiling stm32g0xx_ll_dma.c...
compiling stm32g0xx_hal_dma_ex.c...
compiling stm32g0xx_hal_pwr.c...
compiling stm32g0xx_hal_dma.c...
compiling stm32g0xx_hal_gpio.c...
compiling stm32g0xx_hal_flash_ex.c...
compiling stm32g0xx_hal.c...
compiling stm32g0xx_hal_pwr_ex.c...
compiling stm32g0xx_hal_cortex.c...
compiling stm32g0xx_hal_exti.c...
compiling croutine.c...
../Middlewares/Third_Party/FreeRTOS/Source/event_groups.c(198): error: call to undeclared function '__disable_irq'; ISO C99 and later do not support implicit function declarations [-Wimplicit-function-declaration]
 configASSERT( ( uxBitsToWaitFor & eventEVENT_BITS_CONTROL_BYTES ) == 0 );
 ^
../Core/Inc\FreeRTOSConfig.h(97): note: expanded from macro 'configASSERT'
#define configASSERT( x ) if ((x) == 0) {taskDISABLE_INTERRUPTS(); for( ;; );}
 ^
../Middlewares/Third_Party/FreeRTOS/Source/include/task.h(212): note: expanded from macro 'taskDISABLE_INTERRUPTS'
#define taskDISABLE_INTERRUPTS() portDISABLE_INTERRUPTS()
 ^
../Middlewares/Third_Party/FreeRTOS/Source/portable/RVDS/ARM_CM0\portmacro.h(96): note: expanded from macro 'portDISABLE_INTERRUPTS'
#define portDISABLE_INTERRUPTS() __disable_irq()
 ^
../Middlewares/Third_Party/FreeRTOS/Source/event_groups.c(199): error: call to undeclared function '__disable_irq'; ISO C99 and later do not support implicit function declarations [-Wimplicit-function-declaration]
 configASSERT( uxBitsToWaitFor != 0 );
 ^
../Core/Inc\FreeRTOSConfig.h(97): note: expanded from macro 'configASSERT'
#define configASSERT( x ) if ((x) == 0) {taskDISABLE_INTERRUPTS(); for( ;; );}
 ^
../Middlewares/Third_Party/FreeRTOS/Source/include/task.h(212): note: expanded from macro 'taskDISABLE_INTERRUPTS'
#define taskDISABLE_INTERRUPTS() portDISABLE_INTERRUPTS()
 ^
../Middlewares/Third_Party/FreeRTOS/Source/portable/RVDS/ARM_CM0\portmacro.h(96): note: expanded from macro 'portDISABLE_INTERRUPTS'
#define portDISABLE_INTERRUPTS() __disable_irq()
 ^
../Middlewares/Third_Party/FreeRTOS/Source/event_groups.c(202): error: call to undeclared function '__disable_irq'; ISO C99 and later do not support implicit function declarations [-Wimplicit-function-declaration]
 configASSERT( !( ( xTaskGetSchedulerState() == taskSCHEDULER_SUSPENDED ) && ( xTicksToWait != 0 ) ) );
 ^
.
.
.
.
.
.
.
.
.
.
.
 
#define portDISABLE_INTERRUPTS() __disable_irq()
 ^
../Middlewares/Third_Party/FreeRTOS/Source/portable/RVDS/ARM_CM0/port.c(254): error: call to undeclared function '__enable_irq'; ISO C99 and later do not support implicit function declarations [-Wimplicit-function-declaration]
 portENABLE_INTERRUPTS();
 ^
../Middlewares/Third_Party/FreeRTOS/Source/portable/RVDS/ARM_CM0\portmacro.h(97): note: expanded from macro 'portENABLE_INTERRUPTS'
#define portENABLE_INTERRUPTS() __enable_irq()
 ^
../Middlewares/Third_Party/FreeRTOS/Source/portable/RVDS/ARM_CM0/port.c(259): error: expected '(' after 'asm'
__asm uint32_t ulSetInterruptMaskFromISR( void )
 ^
../Middlewares/Third_Party/FreeRTOS/Source/portable/RVDS/ARM_CM0/port.c(259): error: expected ';' after top-level asm block
__asm uint32_t ulSetInterruptMaskFromISR( void )
 ^
 ;
../Middlewares/Third_Party/FreeRTOS/Source/portable/RVDS/ARM_CM0/port.c(261): error: use of undeclared identifier 'mrs'
 mrs r0, PRIMASK
 ^
../Middlewares/Third_Party/FreeRTOS/Source/portable/RVDS/ARM_CM0/port.c(267): error: expected '(' after 'asm'
__asm void vClearInterruptMaskFromISR( uint32_t ulMask )
 ^
../Middlewares/Third_Party/FreeRTOS/Source/portable/RVDS/ARM_CM0/port.c(267): error: expected ';' after top-level asm block
__asm void vClearInterruptMaskFromISR( uint32_t ulMask )
 ^
 ;
fatal error: too many errors emitted, stopping now [-ferror-limit=]
20 errors generated.
compiling port.c...
compiling stm32g0xx_hal_tim.c...
"Test\Test.axf" - 93 Error(s), 0 Warning(s).
Target not created.
Build Time Elapsed: 00:00:06

This topic has been closed for replies.
Best answer by kaushikbm

Hi Pavel,

I found the solution up here. I had to let go of Keil and install STM32CubeIDE. Now everything is working fine. Thanks for your help :smiling_face_with_smiling_eyes::thumbs_up:

3 replies

Pavel A.
February 19, 2023

It looks that the FreeRTOS is compiled with a wrong style of inline assembly, not intended for Keil V.6 compiler (Clang). It could work perhaps with Keil V.5 compiler (armcc).

kaushikbm
kaushikbmAuthor
Associate II
February 20, 2023

Hey Pavel,

Thank you for the pointer. I tried changing to V5 compiler. Now I'm getting the following error :pensive_face:

It stops after generating 95 errors !

Build started: Project: Test
*** Using Compiler 'V5.03 [Build 76]', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
Build target 'Test'
compiling main.c...
Fatal error: C3906U: Malformed via file 'Test\main.__i'.
Fatal error: C3906U: Malformed via file 'Test\main.__i'.
compiling spi.c...
Fatal error: C3906U: Malformed via file 'Test\spi.__i'.
Fatal error: C3906U: Malformed via file 'Test\spi.__i'.
assembling startup_stm32g030xx.s...
startup_stm32g030xx.s: error: A3906U: Malformed via file 'Test\startup_stm32g030xx._ia'.
compiling usart.c...
Fatal error: C3906U: Malformed via file 'Test\usart.__i'.
Fatal error: C3906U: Malformed via file 'Test\usart.__i'.
compiling app_freertos.c...
Fatal error: C3906U: Malformed via file 'Test\app_freertos.__i'.
Fatal error: C3906U: Malformed via file 'Test\app_freertos.__i'.
.
.
.
.
"Test\Test" - 95 Error(s), 0 Warning(s).
Target not created.
Build Time Elapsed: 00:00:01