Skip to main content
Associate II
February 11, 2025
Question

How to Deploy and Run a C-Based AI Model on Target Hardware?

  • February 11, 2025
  • 0 replies
  • 642 views

Hello everyone,

I have successfully set up and run a C-based AI model on my local development environment using the X-CUBE-AI libraries and a Makefile. The setup involves compiling and executing the model on my local CPU, and I am getting the expected output.

Here is a brief overview of my current setup:

  • Development Environment: Windows with a MinGW-W64 toolchain.
  • Project Structure:
    • A makefile to compile the project.
    • Source files including main.c, and generated model files located in the model directory.
    • X-CUBE-AI libraries located in the cubeai_lib_XX directory.

Now, I am looking to deploy and run this model on my target hardware, which is an STM32 microcontroller. However, I am unsure about the steps needed to transition from running the model on my local CPU to executing it on the target hardware. Unfortunately, I could not find much documentation on this process.

Could anyone provide guidance or resources on:

  1. How to set up the environment for cross-compilation for STM32?
  2. How to transfer the compiled application to the STM32 board?
  3. Any specific configurations or considerations I should be aware of when running the model on STM32?

Any help or pointers to relevant documentation would be greatly appreciated!

Thank you!

This topic has been closed for replies.