Skip to main content
parth kothiya
Associate III
Mar 12, 2022 4:52 AM UTC
Solved

How to create template for my custom STM32 board for STM32CubeMx & IDE?

I have my custom PCB design by using STM32 MCU.

Now i want to know how can i design template for this custom board GPIO pins and other interfaces so when i want to use this i simply select it and all pins are set as template.

every time when i make new project don't need to do all setup again.

similar like any stm32 discovery board all pins are set up already.

How can i do it? which software is used?

This topic has been closed for replies.
TDK
TDKBest answer
Mar 12, 2022 3:38 PM UTC

Can also do File -> Save As to create a duplicate project with the same pin definitions and settings.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

KnarfB
Super User
Mar 12, 2022 6:49 AM UTC

STM32CubeIDE > File > New > STM32 Project from existing .ioc

allows you to create a new project from the settings of an existing one.

hth

KnarfB

TDK
TDKBest answer
Mar 12, 2022 3:38 PM UTC

Can also do File -> Save As to create a duplicate project with the same pin definitions and settings.

"If you feel a post has answered your question, please click ""Accept as Solution""."