Skip to main content
Tank2005
Associate
Mar 9, 2019 8:59 AM UTC
Question

How to create a libusb compatible generic usb device from STM32CubeMX

My environment is NUCLEO-F446RE and TrueSTUDIO / STM32CubeMX.

​On Microchip PIC32MX's framework(MPLAB Harmony), it can make a custom usb device as "Vender".

On the other hand, STM32CubeMX has only options for custom HID and virtual COM devices so I can't define the original device.

 This is an example of a simple WinUSB device demo descriptor output by the microchip framework.

/*******************************************
 * USB Device Layer Descriptors
 *******************************************/
/*******************************************
 * USB Device Descriptor 
 *******************************************/
const USB_DEVICE_DESCRIPTOR deviceDescriptor =
{
 0x12, // Size of this descriptor in bytes
 USB_DESCRIPTOR_DEVICE, // DEVICE descriptor type
 0x0200, // USB Spec Release Number in BCD format
 0x00, // Class Code
 0x00, // Subclass code
 0x00, // Protocol code
 USB_DEVICE_EP0_BUFFER_SIZE, // Max packet size for EP0, see system_config.h
 0x04D8, // Vendor ID
 0x0053, // Product ID
 0x0100, // Device release number in BCD format
 0x01, // Manufacturer string index
 0x02, // Product string index
 0x00, // Device serial number string index
 0x01 // Number of possible configurations
};
 
 
/*******************************************
 * USB Full Speed Configuration Descriptor
 *******************************************/
const uint8_t fullSpeedConfigurationDescriptor[]=
{
 /* Configuration Descriptor */
 
 0x09, // Size of this descriptor in bytes
 USB_DESCRIPTOR_CONFIGURATION, // Descriptor Type
 32,0, //(32 Bytes)Size of the Config descriptor.e
 1, // Number of interfaces in this cfg
 0x01, // Index value of this configuration
 0x00, // Configuration string index
 USB_ATTRIBUTE_DEFAULT | USB_ATTRIBUTE_SELF_POWERED, // Attributes
 50, // Max power consumption (2X mA)
 /* Descriptor for Function 1 - Vendor */ 
 
 /* Interface Descriptor */
 
 0x09, // Size of this descriptor in bytes
 USB_DESCRIPTOR_INTERFACE, // INTERFACE descriptor type
 0, // Interface Number
 0, // Alternate Setting Number
 2, // Number of endpoints in this intf
 0xFF, // Class code
 0xFF, // Subclass code
 0xFF, // Protocol code
 0, // Interface string index
 
 /* Endpoint (OUT) Descriptor */
 
 0x07, // Size of this descriptor in bytes
 USB_DESCRIPTOR_ENDPOINT, // Endpoint Descriptor 
 1 | USB_EP_DIRECTION_OUT, // EndpointAddress ( EP1 OUT )
 USB_TRANSFER_TYPE_BULK, // Attributes
 0x40,0x00, // Max packet size of this EP
 1, // Interval
 
 /* Endpoint (IN) Descriptor */
 
 0x07, // Size of this descriptor in bytes
 USB_DESCRIPTOR_ENDPOINT, // Endpoint Descriptor
 1 | USB_EP_DIRECTION_IN, // EndpointAddress ( EP1 IN )
 USB_TRANSFER_TYPE_BULK, // Attributes
 0x40,0x00, // Max packet size of this EP
 1, // Interval
};

Is there a way to define my own descriptor with STM32CubeMX? Or does STM32 have a library for creating libusb compatible devices? ​

This topic has been closed for replies.