Skip to main content
SLuit.1
Associate III
Sep 9, 2021 12:02 PM UTC
Question

How to configure QUADSPI in stm32h747bi ?

Hi,

I am using stm32h747bi chip in custom board and I want to communicate with GD25Q32C flash memory. I have generated the code for QSPI driver from cubemx. I initialised the GPIO pins as below:

/* Peripheral clock enable */

  __HAL_RCC_QSPI_CLK_ENABLE();

  __HAL_RCC_GPIOE_CLK_ENABLE();

  __HAL_RCC_GPIOF_CLK_ENABLE();

  __HAL_RCC_GPIOA_CLK_ENABLE();

  __HAL_RCC_GPIOB_CLK_ENABLE();

  /**QUADSPI GPIO Configuration

  PE2   ------> QUADSPI_BK1_IO2

  PF8   ------> QUADSPI_BK1_IO0

  PF9   ------> QUADSPI_BK1_IO1

  PA1   ------> QUADSPI_BK1_IO3

  PB2   ------> QUADSPI_CLK

  PB10   ------> QUADSPI_BK1_NCS

  */

  GPIO_InitStruct.Pin = GPIO_PIN_2;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

  GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;

  HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

  GPIO_InitStruct.Alternate = GPIO_AF10_QUADSPI;

  HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = GPIO_PIN_1;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

  GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;

  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_10;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

  GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;

  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

and I have initialised the QUADSPI as below:

static void MX_QUADSPI_Init(void)

{

 /* QUADSPI parameter configuration*/

 hqspi.Instance = QUADSPI;

 hqspi.Init.ClockPrescaler = 5;

 hqspi.Init.FifoThreshold = 4;

 hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;

 hqspi.Init.FlashSize = 21;

 hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_1_CYCLE;

 hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;

 hqspi.Init.FlashID = QSPI_FLASH_ID_1;

 hqspi.Init.DualFlash = QSPI_DUALFLASH_DISABLE;

 if (HAL_QSPI_Init(&hqspi) != HAL_OK)

 {

  Error_Handler();

 }

 else{

 printf("successfully initialised\n");

 }

}

According to the documentaion of STM, QSPI can be configured in 3 different modes but there is not any document how to configure it. Could you please let me know how to configure QSPI in indirect mode.

Another thing after doing all of these I still see that all the functions are inactive in stm32h7xx_hal_qspi.h. In top of the file there is one line #if defined(QUADSPI) and QUADSPI is not defined anywhere so it is inactive. Doesn't HAL_QSPI_Init(&hqspi) defines the QUADSPI and makes it active.

This was not the only place where the QUADSPI was inactive. It was inactive in stm32h7xx_hal_gpio_ex.h.

#if defined(QUADSPI)

#define GPIO_AF9_QUADSPI    ((uint8_t)0x09) /* QUADSPI Alternate Function mapping */

#endif /* QUADSPI */

So how do you configure QUADSPI and make all places where define(QUADSPI) is called active. I cannot go in each page and make those active. I think I am missing something about configuring the QUADSPI.

This is the first time I am working with QUADSPI and stm32. Is there any tutorial where it is guided step by step how to configure QUADSPI in stm32cubeide.

This topic has been closed for replies.

9 replies

Mike_ST
ST Technical Moderator
Sep 9, 2021 12:28 PM UTC

Hello,

>> Another thing after doing all of these I still see that all the functions are inactive in stm32h7xx_hal_qspi.h. In top of the file there is one line #if defined(QUADSPI)

>> and QUADSPI is not defined anywhere so it is inactive.

QUADSPI symbol is defined in stm32h747xx.h.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
SLuit.1
SLuit.1Author
Associate III
Sep 10, 2021 6:41 AM UTC

Yes I know it is defined in stm32h747xx.h but what do I need implement. In every file where if defined(QUADSPI) is called the function is inactive. I downloaded one example project from cubemx and in that one all the functions are active.

I have uncommented #define HAL_QSPI_MODULE_ENABLED and I have initialised the QUADSPI in main.c as I have explained above. Compiler is not showing any error but all the functions, macros and typedefs are inactive in stm32h7xx_hal_qspi.h. 

And the functions were inactive wherever #if defined(QUADSPI) was called.

I don't know if I can make you understand or not.

Tesla DeLorean
Guru
Sep 9, 2021 1:09 PM UTC

Check stm32h7xx_hal_conf.h

#define HAL_QSPI_MODULE_ENABLED

And at the compiler command line the MCU is passed as a define

STM32H747xx

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SLuit.1
SLuit.1Author
Associate III
Sep 10, 2021 6:47 AM UTC

Yes I uncommented #define HAL_QSPI_MODULE_ENABLED and compiled the program with initialisation of QUADSPI. Compiler is not showing any error but all the fucntions,macros and typedefs are inactive in stm32h7xx_hal_qspi.h.

And the functions were inactive where ever  #if defined(QUADSPI) were called.

I don't know if I can make you understand or not but I want to make all of them active.

I downloaded one example project from cubemx to check it and all of those were active in example project. I tried to find the difference but I could not. So I think I am missing something and don't know what.

Mike_ST
ST Technical Moderator
Sep 10, 2021 8:13 AM UTC

>> In every file where if defined(QUADSPI) is called the function is inactive.

What make you think that the code is not compiled ? What actual error message do you get ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.