Skip to main content
FSchm.7
Associate
Dec 19, 2022 7:59 PM UTC
Solved

How to change the Pull-up/Pull-down behavior in the stm32CubeMx Software.

 I am using Linux Linux kubuntu 22.10 5.19.0-26-generic and when I click on the GPIO Pull-up/Pull-down column elements nothing happens except the color of the row changes.

This topic has been closed for replies.
Karl Yamashita
Karl YamashitaBest answer
Principal
Dec 19, 2022 8:29 PM UTC

You have to scroll down or drag the configuration window up a little bit to see the parameters

0693W00000WLM4KQAX.png

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source

3 replies

MM..1
Super User
Dec 19, 2022 8:21 PM UTC

Click on System Core and GPIO.

Karl Yamashita
Karl YamashitaBest answer
Principal
Dec 19, 2022 8:29 PM UTC

You have to scroll down or drag the configuration window up a little bit to see the parameters

0693W00000WLM4KQAX.png

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
FSchm.7
FSchm.7Author
Associate
Dec 19, 2022 9:22 PM UTC

@Community member​  thanks a lot I just didn't see the scroll bar