Skip to main content
Ekim.1
Associate III
June 2, 2022
Solved

How to change chip selection after a project is created

Hello, I'm programming using STM32H753. But I realized that the chip I chose when I was creating the project was STM32H743. Is there any way to change the chip settings in a project that has already been created? Should we re-create a new project unconditionally? Answer me. Thank you.

This topic has been closed for replies.
Sara BEN HADJ YAHYA
ST Technical Moderator
June 2, 2022

Hello @Ekim.1​ ,

Thanks for your feedback,

There are two methods to change an MCU by CubeMX. For more details, please check my answer in this thread Changing from STM32F769NIHx to STM32F769BGTx.

PS: Unfortunately the  List Pinout Compatible MCUs is bugged in v6.5.0 but it will be fixed. I would advice you to use the import method if you are working with v6.5.0.

I hope this helps !

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

5 replies

Anil3
Associate III
June 2, 2022

Hi @Ekim.1​ 

I think there is no such kind of option to change the chip, if once the project is created .ioc file will be generated which is particular for that controller only.

If you think that this is best, select as best so that other's can find out easily.

KnarfB
Super User
June 2, 2022

Good news: there is a way in STM32CubeMX by pressing Alt+L or drop down the Pinout menu in the Pinout & Config tab.

Bad news: Some reported that the feature is sluggish or even broken in the current version, so you may try several times.

hth

KnarfB

Michael E
ST Technical Moderator
June 2, 2022

Hi @Ekim.1​ ,

Unfortunately, for the moment, the STM32CubeMX is not able to migrate a project to another STM32.

Best Regards

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
VZhik
Visitor II
June 2, 2022

You can create a new empty project and import a old one

Sara BEN HADJ YAHYA
ST Technical Moderator
June 2, 2022

Hello @Ekim.1​ ,

Thanks for your feedback,

There are two methods to change an MCU by CubeMX. For more details, please check my answer in this thread Changing from STM32F769NIHx to STM32F769BGTx.

PS: Unfortunately the  List Pinout Compatible MCUs is bugged in v6.5.0 but it will be fixed. I would advice you to use the import method if you are working with v6.5.0.

I hope this helps !

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.