Skip to main content
ZZqk
Associate
Jun 2, 2019 11:49 AM UTC
Solved

How to add BSP library cubemxide?

Hi, I try to use stm32f429 lcd screen. for this i need to add bsp library in my project and then use some .c file like sdram.c lcd.c etc. 

Can someone explain how can i add this library ?

What I'm trying to do is in the video on the link, but he's using Keil.

https://www.youtube.com/watch?v=u_TVAudWabI

Is there another method for controlling the LCD? Only using cubemx.

I just want to print the word alone on the screen.

Thank you.

This topic has been closed for replies.
Ethan HUANG
Ethan HUANGBest answer
ST Employee
Jun 5, 2019 2:56 AM UTC

I think you could follow the attachment to deal with "adding BSP into your CubeIDE project" in a quick way so you could start from a BSP added code base.

4 replies

ZZqk
ZZqkAuthor
Associate
Jun 3, 2019 6:51 PM UTC

I still need a help. hopefully someone helps.

Ethan HUANG
Ethan HUANGBest answer
ST Employee
Jun 5, 2019 2:56 AM UTC

I think you could follow the attachment to deal with "adding BSP into your CubeIDE project" in a quick way so you could start from a BSP added code base.

CDew.1
Associate III
Jan 30, 2020 2:45 PM UTC

Hi ZZqk - did you find an answer?

I followed Ethan HUANG's answer. It fixed almost all of the undefined references, but createFramewin() (in GUI_App.c) is still undefined.

victagayun
Senior III
Aug 7, 2020 1:43 AM UTC

0693W000003OgEoQAK.jpgYou may still need to add it in the GCC compiler include path

 0693W000003OgEjQAK.jpg

and check if added in path and symbols