Skip to main content
Curtis.Allen
Associate III
Sep 20, 2020 5:53 PM UTC
Question

How do you install X-CUBE-AWS pack in STM32CubeMX?

  • I downloaded en.x-cube-aws_v2-0-0.zip
  • open STM32CumeMX
  • goto "Manage Embedded Software packages
  • select "From Local..."

The message says that the ZIP does not contain information it needs to install.

This topic has been closed for replies.

8 replies

Guillaume K
ST Employee
Sep 21, 2020 12:36 PM UTC

X-CUBE-AWS is not a "CMSIS pack".

Just unzip the X-CUBE-AWS .zip file at root of c:\ and use STM32CubeIDE's "import" function to develop with it.

JWang.10
Associate
Sep 22, 2020 3:09 AM UTC

That package seems for STM32L4, I now use STM32F217+FreeRTOS and a developing project created by CubeIDE.

I am wandering the right way to integrate x-cube-aws into my project, any suggestion?

Guillaume K
ST Employee
Sep 22, 2020 12:02 PM UTC

Are you talking of X-CUBE-AWS 2.0 ?

X-CUBE-AWS 2.0 is based on Amazon FreeRTOS. It is ported only on B-L4S5I-IOT01. It uses several features of B-L4S5I-IOT01 that will be difficult to have on STM32F217: STSAFE, WiFi, ... I don't think it's feasible.

Curtis.Allen
Associate III
Sep 21, 2020 4:27 PM UTC

What if you don't use STM32CubeIDE for development?

I would like to pick this as a package to be included in a STMCubeMX generated "Makefile" project. Are any of the components like the Amazon FreeRTOS available as a package?

Guillaume K
ST Employee
Sep 22, 2020 12:10 PM UTC

in X-CUBE-AWS 2.0 .zip file there are STM32CubeIDE and IAR EWARM project files.

Currently Amazon FreeRTOS is not available as a CMSIS package for STM32.