Skip to main content
Mike xx
Associate III
Nov 30, 2020 4:58 PM UTC
Solved

How do I setup EXTI[15:10] interrupts without enabling them until required?

If I tick the enable box in STM32CUBEMX the interrupt is enabled when MX_GPIO_Init() is executed. Since this is prior to the initialisation of FreeRTOS queues etc this turns into a disastrous mess.

If I leave the box unticked then everything assoociated with this interrupt must be written manually.

It's a shame that the interrupt can't be setup in the MX and then manually enabled when the appropriate FreeRTOS task becomes active.

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
Dec 1, 2020 1:37 AM UTC

No, it is not a shame, you just need to know the trick.

Insert the following line before the cube generated code that configures NVIC interrupts:

__set_BASEPRI(configMAX_SYSCALL_INTERRUPT_PRIORITY);

This will disable all interrupts that should not occur before FreeRTOS scheduler starts.

When it starts and any thread runs, BASEPRI will automatically return to 0 and these interrupts will be unmasked.

And the life is good again =)

Note: assuming that priority of HAL timer interrupt is higher than SYSCALL_INTERRUPT_PRIORITY. The HAL tick is used to detect timeouts during initialization of many HAL drivers so it should normally work as soon as the HAL starts it.

-- pa

5 replies

waclawek.jan
Super User
Nov 30, 2020 8:34 PM UTC

> If I leave the box unticked then everything assoociated with this interrupt must be written manually.

And why would that be a problem? It's a write to two or three registers, and then enabling the interrupt in NVIC. Hardly a challenge.

Cube/CubeMX inevitably caters only for a limited subset of the virtually infinite modes of usage of the peripherals. There's just so many things you can control by clicking. I'm sure ST is willing to provide you a dedicated clicking interface for whatever functionality you desire, if you present a significant buying power (as expressed in $M+).

JW

Mike xx
Mike xxAuthor
Associate III
Dec 1, 2020 2:00 AM UTC

Yes I appreciate it can't be the singing and dancing solution for everyone all the time. But when FreeRTOS is used, where queues are typically filled from interrupts it becomes a certain failure for anyone using FreeRTOS.

Pavel A.
Pavel A.Best answer
Dec 1, 2020 1:37 AM UTC

No, it is not a shame, you just need to know the trick.

Insert the following line before the cube generated code that configures NVIC interrupts:

__set_BASEPRI(configMAX_SYSCALL_INTERRUPT_PRIORITY);

This will disable all interrupts that should not occur before FreeRTOS scheduler starts.

When it starts and any thread runs, BASEPRI will automatically return to 0 and these interrupts will be unmasked.

And the life is good again =)

Note: assuming that priority of HAL timer interrupt is higher than SYSCALL_INTERRUPT_PRIORITY. The HAL tick is used to detect timeouts during initialization of many HAL drivers so it should normally work as soon as the HAL starts it.

-- pa

Mike xx
Mike xxAuthor
Associate III
Dec 1, 2020 2:35 AM UTC

I can see the significance of your note. The current priority set by the FreeRTOS middleware is now 15. Until the latest version of MX it was 0, so unmaskable. I have no idea why the change but of course it does mean that HAL_Delay no longer works.