Skip to main content
Ali Pourmohammad
Associate II
Jun 6, 2017 5:48 PM UTC
Question

How can I use audio codec in STM32CubeMX?

Posted on June 06, 2017 at 19:48

Hello.

I use STM32CubeMX for programming of a STM32F407 Discovery board.

I want to play a sound using audio codec.

Unfortunately I can't communicate with codec by I2C and I2S.

There is no any sound in headphone.

Is there any simple example for Audio Playing in 

STM32CubeMX without using DMA or Interrupt or USB?

Maybe using a MEMS Mic?

#audio-playing-in-stm32cubemx
This topic has been closed for replies.

5 replies

ST Technical Moderator
Jun 7, 2017 12:37 PM UTC
Posted on June 07, 2017 at 14:37

Hi

Pourmohammad.Ali

,

There is no examples available with STM32CubeMx, wehave

the Audio example but with DMA or interrupt within

/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fen%2Fembedded-software%2Fstm32cubef4.html

firmware package available at this path:

STM32Cube_FW_F4_V1.0\Projects\STM32F4-Discovery\Applications\Audio\Audio_playback_and_record

Hopecommunity' users will helpyou with working example.

Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Ali Pourmohammad
Associate II
Jun 7, 2017 4:26 PM UTC
Posted on June 07, 2017 at 16:26

Dear Imen, Hello.

Thanks a lot for your help.I tried that example but I couldn't communicate with the codec.First I want to communicate with the codec.I use STM32CubeMX compiler and Hal drivers.I activated I2S3 and I2C1 then tried to read the ID register of the codec but it didn't work.I tried it using two different STM32F407 discovery board.May you guide me how can I read the ID register first?

Best RegardsAli Pourmohammad