Skip to main content
howard n2wx
Associate III
Jan 11, 2017 5:02 PM UTC
Solved

How can I prevent stm32cubemx v1.18 from deleting my files from the project Src directory and the EWARM project? [Solved with 4.19]

Posted on January 11, 2017 at 18:02

In an IAR/EWARM environment, when I use STM32CubeMX 4.18.0 Project/Generate Code function the program seems to correctly generate its own files but deletes user (that is, my files) from both the EWARM project and from the file system.

It appears this was reported for some earlier CubeMX versions too (

https://community.st.com/0D50X00009Xkf15SAB

for ex). Anyone else suffer and fix this issue? 

EDIT 170112 confirmed as a regression --- non-cubic sources preserved with 4.16.0. Not sure about 4.17.0.....

This topic has been closed for replies.
howard n2wx
howard n2wxBest answer
Associate III
Feb 2, 2017 5:10 PM UTC
Posted on February 02, 2017 at 17:10

I'm not seeing the problem with 4.19; please disregard

2 replies

ST Technical Moderator
Jan 12, 2017 7:58 AM UTC
Posted on January 12, 2017 at 08:58

Hello

goldstein.howard

‌,

Your issueis reportedto CubeMx team for further investigation.

Thank you for highlighting it and Sorry for the inconvenience it may bring.

Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
howard n2wx
howard n2wxAuthorBest answer
Associate III
Feb 2, 2017 5:10 PM UTC
Posted on February 02, 2017 at 17:10

I'm not seeing the problem with 4.19; please disregard