Skip to main content
This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
May 1, 2019 7:12 PM UTC

USART1 PA9/PA10 is not viable due to a capacitor on one of the lines.

Use USART6 PC6/PC7

The USART signals at CMOS levels, this is not compatible with RS232, you will need a MAX3232 type device to shift levels if using RS232 connectivity.

You may use a USB-to-CMOS Serial adapter/dongle, FTDI or SiLabs type chips.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
alouni bargougui
Associate
May 1, 2019 8:21 PM UTC

thank you Clive Two.Zero

i used usb ttc adaptator

i need to use TIM or not ?

Tesla DeLorean
Guru
May 1, 2019 10:19 PM UTC

The USART peripheral functions independently of the TIM and other peripherals. Your library may established other requirements for timeouts etc, ie HAL with SysTick

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..