Skip to main content
ab_nurd
Associate II
May 5, 2021 12:59 PM UTC
Question

Hostname of STM32F7 with FW 1.16.1 and LWIP v 2.1.2 is not changable

Hello,

I have generated code for STM32F7 using STM32CubeMX with firmware package version 1.16.1 and lwIP version 2.1.2.

In ethernetif_init function of ethernetif.c file, I have changed default value of netif->hostname.(LWIP_NETIF_HOSTNAME is already enabled) But when I search the active nodes on network using "arp-scan --localnet" I see the hostname of my STM32 as "STMicroelectronics SRL" and not the one which was set in code.

How can the default hostname be changed?

Thanks.

Abhijeet

This topic has been closed for replies.

2 replies

Khouloud OTHMAN
Associate
May 21, 2021 5:54 PM UTC

Hello @Community member​,

First le me welcome you to the STM32 Community and apologize for the late reply :smiling_face_with_smiling_eyes:

In order to avoid any misunderstanding could you please detail more the issue.

Do you mean that even after enabling LWIP_NETIF_HOSTNAME  through STM32CubeMX interface, it will not be correctly set to 1 in the generated lwipopts.h ?

Normally, LWIP_NETIF_HOSTNAME parameter should be defined to 1 in your lwipopts.h. The default host name value is "lwip" ,please refer to 'ethernetif_init()' function of ethernetif.c file:

#if LWIP_NETIF_HOSTNAME
 /* Initialize interface hostname */
 netif->hostname = "lwip";
#endif /* LWIP_NETIF_HOSTNAME */

Then you can change it by your preferred host name value, or you can call 'netif_set_hostname()' after the initialization to override the default name.

Furthermore, you'll find linked the User Manual detailing the process of developing applications on STM32Cube with LwIP TCP/IP stack.

Your feedback will be very helpful to discern the problem :)

Khouloud.

ab_nurd
ab_nurdAuthor
Associate II
Aug 7, 2021 8:38 PM UTC

Hello Khouloud,

we assigned our company specific MAC address in low_level_init function, after which the hostname was set to our company name (setting hostname using lwIP had still no effect though).

Thanks & Regards,

Abhijeet