Skip to main content
Scotty55
Associate III
Nov 18, 2019 4:58 PM UTC
Question

Hello, for a STM32F474RBT device, STM32CubeMX V.5.4.0 with Firmware V.1.1.0 allows to put OPAMP1_INP and COMP1_INP on a single port PA1. Is this really a valid configuration, or is it a CubeMX bug?

..

This topic has been closed for replies.

2 replies

Andrea Canepa
Senior
Nov 18, 2019 5:16 PM UTC

It is not a BUG. Both in F3 and in G4 it is possible to use the same analog input pin for more analog peripheral.

This can help to reduce the number of pins. You can use the MCU manual to see which pins have matched that particular analog peripheral.

Regards

Andrea

Scotty55
Scotty55Author
Associate III
Nov 18, 2019 6:12 PM UTC

Thank you very much! I had some trouble with CubeMX 5.4 configuring a STM32F334, ended up with going back to version 5.3...

best regards - Scotty