Question
Hello all, I used Demonstrator GUI and CubeMXPRG for several projects till now without any issues. I tick "jump to user code" after flashing and this worked all along. However this feature is giving problems in both the utilities. The code gets
programmed and thereafter either the controller resets or simply hangs. I tried both GUI and Cube programmer. The result is the same. If I change the BOOT0 and BOOT1 pins to FLASH execute mode and apply power the code works but changing the jumpers many times is eating into my time and testing time has increased enormously. I have switched to Windows 11 recently, but even after that I used the applications without any issue. Now I am facing this issue and I have some deadlines to meet. Can some please hep me resolve this issue ASAP. Thank you.