Skip to main content
Martin Franke
Associate II
May 27, 2021 9:55 PM UTC
Question

Heap_x.c file not in GPDSC file generated by STM32CubeMX

Hi, I've generated a project using STM32CubeMX for the STM32G030C8Tx and I've included FREERTOS. The heap_x file is not listed in the GPDSC file. I think this is a bug, note someone else appears to have had the same issue here: Topic: Error undefined reference to `pvPortMalloc and `vPortFree' | Sysprogs

Attached is my .ioc file and GPDSC file (I had to change it to a txt file to upload).

This topic has been closed for replies.

5 replies

Houda GHABRI
ST Employee
Jun 1, 2021 1:21 PM UTC

Hi @Martin Franke​ 

Let me be sure that I understand the issue, is that Heap_x.c files are not generated in project folder?

In my case ,when I load your ioc and generate using STM32CubeMX , Heap_1.c to Heap_5.c are generated under :

Middlewares\Third_Party\FreeRTOS\Source\portable\MemMang\

Please tell me if I miss something?

Houda

Martin Franke
Associate II
Jun 1, 2021 4:10 PM UTC

Hello @Houda GHABRI​,

Thanks for looking into this. The files are generated correctly, but there is no reference to them in the gpdsc file. I'm using VisualGDB with CubeMX and when I generate a new project it doesn't automatically reference them since it pulls all its references from the gpdsc file. It's not a major bug since I can manually add them but might be really frustrating for someone. It wasn't immediately obvious to me where the problem was when I began the project.

Thanks,

Martin

Houda GHABRI
ST Employee
Jun 2, 2021 12:51 PM UTC

Hi @Martin Franke​ ,

Thanks I catch the point.

The issue is reproduced and internal ticket is submitted to STM32CubeMX development team to be fixed as soon as possible.

Houda

Martin Franke
Associate II
Jun 2, 2021 6:58 PM UTC

Hello @Houda GHABRI​ ,

Thank you very much for taking time to submit this to the development team.

Martin

Houda GHABRI
ST Employee
Jun 3, 2021 8:04 AM UTC

Hi @Martin Franke​ ,

Thanks to you for bringing this error to our attention.

Houda