Skip to main content
GModu.1
Associate
Dec 16, 2019 11:36 PM UTC
Question

HAL_OSPIM_Config and zero-initialized members of OSPIM_CfgTypeDef

I have to configure OCTOSPI2 in Single Mode and only three pins managed directly from peripheral: SI, SO anche CLK.

The code generated from MX is the following:

static void MX_OCTOSPI2_Init(void)
{
 ...
 OSPIM_CfgTypeDef OSPIM_Cfg_Struct = {0};
 ...
 OSPIM_Cfg_Struct.ClkPort = 1;
 OSPIM_Cfg_Struct.IOLowPort = HAL_OSPIM_IOPORT_2_LOW;
 if (HAL_OSPIM_Config(&hospi2, &OSPIM_Cfg_Struct, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }

The function HAL_OSPIM_Config() checks validity of all members of OSPIM_Cfg_Struct:

HAL_StatusTypeDef HAL_OSPIM_Config(OSPI_HandleTypeDef *hospi, OSPIM_CfgTypeDef *cfg, uint32_t Timeout)
{
 ...
 /* Check the parameters of the OctoSPI IO Manager configuration structure */
 assert_param(IS_OSPIM_PORT(cfg->ClkPort));
 assert_param(IS_OSPIM_PORT(cfg->DQSPort));
 assert_param(IS_OSPIM_PORT(cfg->NCSPort));
 assert_param(IS_OSPIM_IO_PORT(cfg->IOLowPort));
 assert_param(IS_OSPIM_IO_PORT(cfg->IOHighPort));

So this function fires an assert, because DQSPort and NCSPort are zero, but they should be 1 or 2.

Is this a bug in MX auto-generated code?

This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
Jan 28, 2020 3:45 PM UTC

Hello @GModu.1​ ,

I assume that the assert checks applied on HAL_OSPIM_Config (stm32l4xx_hal_ospi.c) should depend on the selected mode to configure the OctoSPI.

This is shared internally with our development team for further check & review.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.