Skip to main content
PDaum.1
Associate
Dec 8, 2021 10:01 PM UTC
Solved

GPIO_InfiniteLedToggling_init NUCLEO-144 Start Project Issue

I receive the following error trying to start the project: Error Downloading the following files: stm32cube_fw_u5_v102.zip (Target directory already exists). The zip file is in fact there. But I can't proceed any further.

This topic has been closed for replies.
PDaum.1
PDaum.1Best answer
Associate
Dec 9, 2021 7:42 PM UTC

Thanks for your response. I was able to get things working by uninstalling the MX and IDE components and then reinstalling by explicitly right clicking the install file and choosing "Run as Administrator". I missed doing that the first time I installed.

3 replies

PDaum.1
PDaum.1Author
Associate
Dec 8, 2021 10:35 PM UTC

Just a bit more information: I used the embedded package manager to try updating from local and navigated to the zip file but received an error message that I cannot select a file in an STM32CubeMx repository.

TDK
Dec 8, 2021 11:30 PM UTC

Add the package using the embedded manager instead. Don't try to add it manually. If you've already done so, undo what you've done.

Help -> Manage Embedded...

Use the Example Selector to open an example from within STM32CubeIDE.

"If you feel a post has answered your question, please click ""Accept as Solution""."
PDaum.1
PDaum.1AuthorBest answer
Associate
Dec 9, 2021 7:42 PM UTC

Thanks for your response. I was able to get things working by uninstalling the MX and IDE components and then reinstalling by explicitly right clicking the install file and choosing "Run as Administrator". I missed doing that the first time I installed.