Skip to main content
SKuma.14
Visitor II
Nov 10, 2020 2:10 PM UTC
Solved

Generic makefile using stm32cubeide

Hi All,

How do I generate a generic Makefile from STM32Cube ide? Preferably for L56 series. Currently when I create a project the Makefile option under toolchains inside the cubemx is grayed out. The CubeMX is installed as part of IDE.

thanks,

This topic has been closed for replies.
Khouloud ZEMMELI
Khouloud ZEMMELIBest answer
ST Employee
Nov 10, 2020 2:19 PM UTC

Hello @SKuma.14​ 

Using CubeIDE, it's not possible to change the Toolchain other than CubeIDE, please use CubeMX standalone if you need to use other Toolchain/IDE.

For L5, only EWARM, Keil and CubeIDE are supported.

Best Regards,

Khouloud

1 reply

Khouloud ZEMMELI
Khouloud ZEMMELIBest answer
ST Employee
Nov 10, 2020 2:19 PM UTC

Hello @SKuma.14​ 

Using CubeIDE, it's not possible to change the Toolchain other than CubeIDE, please use CubeMX standalone if you need to use other Toolchain/IDE.

For L5, only EWARM, Keil and CubeIDE are supported.

Best Regards,

Khouloud