Associate
Jul 1, 2019 6:31 PM UTC
Solved
Generating Code Does Not Copy Files to STM32F7xx_HAL_Driver
- 1 reply
- 792 views
Attached is the IOC file I am using. When I generate the project, the STM32F7xx_HAL_Driver directory has a few folders inside of it, but none of the HAL files, including the stm327xx_hal.h file which prevents compiling from working. I have the "Copy all used libraries into the project folder" option selected. Why are none of the HAL files copied into the project directory?