Skip to main content
Associate
May 14, 2026 1:48 PM UTC
Solved

generated CMakeLists.txt for STM32WBA25 BLE projects fails to link

missing --start-group around WBA2_LinkLayer_BLE_Full_lib.

Environment

  • STM32CubeMX version: 6.17.0
  • STM32CubeWBA firmware package: 1.9.0
  • Target device: STM32WBA25CG (NUCLEO-48 board)
  • Toolchain: GNU Tools for STM32 14.3.1+st.2 (arm-none-eabi-gcc/ld)
  • Build system: CMake (toolchain selected via "CMake" in CubeMX project settings)
  • Host OS: Windows 11

Steps to reproduce

  1. Create a new STM32CubeMX project for STM32WBA25 (NUCLEO board).
  2. Enable BLE (peripheral role, BLE_Full stack).
  3. In Project Manager → Toolchain/IDE, select CMake.
  4. Generate code.
  5. Build with the generated CMakeLists (e.g. cube-cmake --build build/Debug).

Expected Build links cleanly.

Actual Link fails with:

ld.exe: stm32wba_ble_stack_full.a(le_ctrl.o): in function `LECTRL_LL_Init':
 le_ctrl.c:(.text.LECTRL_LL_Init+0xa): undefined reference to `ll_ble_events_init'
ld.exe: (ll_ble_events_init): Unknown destination type (ARM/Thumb) in
 stm32wba_ble_stack_full.a(le_ctrl.o)
 le_ctrl.c:(.text.LECTRL_LL_Init+0xa): dangerous relocation: unsupported relocation

Root cause The generated cmake/stm32cubemx/CMakeLists.txt emits the BLE archives in this order in MX_LINK_LIBS:

set(MX_LINK_LIBS
 :WBA2_LinkLayer_BLE_Full_lib.a
 :stm32wba_ble_stack_full.a
 ...
)

which produces the link line:

... -l:WBA2_LinkLayer_BLE_Full_lib.a -l:stm32wba_ble_stack_full.a -lm

The two archives are mutually dependent:

  • stm32wba_ble_stack_full.a (le_ctrl.o) → LECTRL_LL_Init → references ll_ble_events_init
  • WBA2_LinkLayer_BLE_Full_lib.a (ll_ble_events.o) → defines ll_ble_events_init → references ll_sys_ble_cntrl_init (defined in project sources / ll_sys_startup.c)

GNU ld only scans static archives in the order they appear and does not re-scan earlier archives by default. When stm32wba_ble_stack_full.a is processed and pulls in le_ctrl.o, the new undefined reference to ll_ble_events_init cannot be resolved because the link-layer archive has already been scanned. The follow-up Unknown destination type (ARM/Thumb) is a secondary error from ld attempting to emit an interworking veneer to a still-unresolved symbol.

I confirmed ll_ble_events_init is present and defined in WBA2_LinkLayer_BLE_Full_lib.a (arm-none-eabi-nm shows T ll_ble_events_init, size 8 bytes — a small Thumb-2 trampoline into ll_sys_ble_cntrl_init). So this is purely a link-ordering bug, not a missing-library issue.

Suggested fix in the CubeMX CMake template Wrap the two BLE archives in --start-group/--end-group so ld re-scans until all references are resolved:

set(MX_LINK_LIBS
 -Wl,--start-group
 :WBA2_LinkLayer_BLE_Full_lib.a
 :stm32wba_ble_stack_full.a
 -Wl,--end-group
 STM32_Drivers
 ${TOOLCHAIN_LINK_LIBRARIES}
 Utilities STM32_WPAN Common
)

(Or, for CMake ≥ 3.24, use $<LINK_GROUP:RESCAN,...>.) Simply swapping the order works for this specific symbol chain too, but the group is robust against any future circular dependency between the link-layer and BLE-stack archives. The IAR/MDK/Makefile templates appear unaffected because of how they emit the link command.

Workaround Manually edit cmake/stm32cubemx/CMakeLists.txt after each regeneration to add the --start-group/--end-group flags.

Souhaib MAZHOUDBest answer
ST Technical Moderator
Jul 1, 2026 9:32 AM UTC

Hello ​@oriinbar 

This issue has been fixed in the latest version of STM32CubeMX 6.18.0 

Download STM32CubeMX6.18.0 from this link. 

Regards,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

4 replies

ST Technical Moderator
May 14, 2026 3:09 PM UTC

Hello @oriinbar 

Could you please provide your ioc in order to investigate the issue?

KR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
oriinbarAuthor
Associate
May 18, 2026 10:33 AM UTC

sure - see attached.

i simply tried to follow your hands on video.

ST Technical Moderator
May 20, 2026 4:03 PM UTC

Hello @oriinbar 

Thank you for sharing your feedback and the workaround. We truly appreciate your helpful explanation. This issue has already been escalated internally to the dedicated team and tracked by Internal ticket number: CDM0059620 (This is an internal tracking number and is not accessible or usable by customers.)

A fix will be implemented in the upcoming releases of STM32CubeMX.

BR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Souhaib MAZHOUDBest answer
ST Technical Moderator
Jul 1, 2026 9:32 AM UTC

Hello ​@oriinbar 

This issue has been fixed in the latest version of STM32CubeMX 6.18.0 

Download STM32CubeMX6.18.0 from this link. 

Regards,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.