Skip to main content
alexander2399
Associate II
July 15, 2024
Solved

"generate code" fails due to java error.

When I try to generate code I am getting "eclipsec" error pop=up referring me to a log file. The file content is attached below. I have uninstalled all the STM32 applications and reinstalled just MX 6.12.0, but error is still here.

 

!SESSION 2024-07-15 17:37:34.297 -----------------------------------------------
eclipse.buildId=unknown
java.version=17.0.11
java.vendor=Eclipse Adoptium
BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=en_US
Framework arguments:  -application com.st.stm32cube.ide.common.services.mx.rcpApp -rmiServerPort 8435 -projectUpdate -buildType exec -src cube -cubeScratchFile C:\GIT_REPS\PROJECTS\JefCore\SPLIT\FIRMWARE\Simulator\F3discovery\MX\mx.scratch
Command-line arguments:  -os win32 -ws win32 -arch x86_64 -application com.st.stm32cube.ide.common.services.mx.rcpApp -data C:\Users\panasyuk\.stm32cubeide\.workspace_5374180911736407778 -rmiServerPort 8435 -projectUpdate -buildType exec -src cube -cubeScratchFile C:\GIT_REPS\PROJECTS\JefCore\SPLIT\FIRMWARE\Simulator\F3discovery\MX\mx.scratch
 
!ENTRY org.eclipse.osgi 4 0 2024-07-15 17:37:37.072
!MESSAGE Application error
!STACK 1
java.lang.reflect.InaccessibleObjectException: Unable to make boolean sun.nio.fs.WindowsFileAttributes.isDirectoryLink() accessible: module java.base does not "opens sun.nio.fs" to unnamed module @55a609dd
at java.base/java.lang.reflect.AccessibleObject.checkCanSetAccessible(AccessibleObject.java:354)
at java.base/java.lang.reflect.AccessibleObject.checkCanSetAccessible(AccessibleObject.java:297)
at java.base/java.lang.reflect.Method.checkCanSetAccessible(Method.java:199)
at java.base/java.lang.reflect.Method.setAccessible(Method.java:193)
at org.eclipse.core.internal.filesystem.local.nio.DosHandler.isDirectoryLink(DosHandler.java:80)
at org.eclipse.core.internal.filesystem.local.nio.DosHandler.fetchFileInfo(DosHandler.java:61)
at org.eclipse.core.internal.filesystem.local.LocalFileNativesManager.fetchFileInfo(LocalFileNativesManager.java:89)
at org.eclipse.core.internal.filesystem.local.LocalFile.fetchInfo(LocalFile.java:181)
at org.eclipse.core.filesystem.provider.FileStore.fetchInfo(FileStore.java:260)
at org.eclipse.core.internal.utils.FileUtil.realPath(FileUtil.java:136)
at org.eclipse.core.internal.utils.FileUtil.realURI(FileUtil.java:191)
at org.eclipse.core.internal.localstore.FileSystemResourceManager.setLocation(FileSystemResourceManager.java:1098)
at org.eclipse.core.internal.resources.Project.internalSetDescription(Project.java:861)
at org.eclipse.core.internal.resources.Project.create(Project.java:316)
at com.st.stm32cube.common.projectcreation.core.ProjectUtilities.getProject(ProjectUtilities.java:532)
at com.st.stm32cube.common.projectcreation.core.ProjectUtilities.getProject(ProjectUtilities.java:494)
at com.st.stm32cube.ide.common.services.adapted.core.project.ProjectUpdateRcpServiceProcess.doProjectUpdate(ProjectUpdateRcpServiceProcess.java:132)
at com.st.stm32cube.ide.common.services.adapted.core.project.ProjectUpdateRcpServiceProcess.run(ProjectUpdateRcpServiceProcess.java:120)
at com.st.stm32cube.ide.common.services.mx.core.project.ProjectUpdateRcpService.doProjectUpdate(ProjectUpdateRcpService.java:171)
at com.st.stm32cube.ide.common.services.mx.core.project.ProjectUpdateRcpService.run(ProjectUpdateRcpService.java:166)
at com.st.stm32cube.ide.common.services.mx.update.MxUpdateProjectRcpService.run(MxUpdateProjectRcpService.java:117)
at com.st.stm32cube.ide.common.services.mx.update.MxUpdateProjectRcpService.run(MxUpdateProjectRcpService.java:109)
at com.st.stm32cube.ide.common.services.mx.rcp.CubeIdeServices.start(CubeIdeServices.java:96)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:208)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:402)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:77)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:568)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:651)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:588)
at org.eclipse.equinox.launcher.Main.run(Main.java:1459)
 
!ENTRY org.eclipse.core.resources 2 10035 2024-07-15 17:37:37.095
!MESSAGE The workspace will exit with unsaved changes in this session.

 

This topic has been closed for replies.
TDK
TDKBest answer
July 16, 2024

Hmm, works fine for me. Without being able to duplicate the error, it's difficult to help much. Try starting from a new project and progressively assign pins and functions and generate code see where it starts to fail. Might shed some insight. Or maybe starting from a new project will work. Not a great answer but that's all I got. Good luck.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

TDK
July 15, 2024

Can you share the IOC causing the issues?

Can you generate a new/blank IOC file and generate code?

Windows 11 64-bit?

"If you feel a post has answered your question, please click ""Accept as Solution""."
alexander2399
Associate II
July 16, 2024

Attached is the IOC file. I can generate code from an empty IOC for the same board without an error. Windows 10 64-bit.

 

Thanks!

TDK
TDKBest answer
July 16, 2024

Hmm, works fine for me. Without being able to duplicate the error, it's difficult to help much. Try starting from a new project and progressively assign pins and functions and generate code see where it starts to fail. Might shed some insight. Or maybe starting from a new project will work. Not a great answer but that's all I got. Good luck.

"If you feel a post has answered your question, please click ""Accept as Solution""."