Skip to main content
Associate II
Dec 13, 2024 2:28 PM UTC
Question

FreeRTOS SysTick_Handler missing

Moved from MPUs forum; STM32F072 is an MCU - not an MPU.


Hi,

I've just started a new project for a STM32F072 chip using STM32CubeIDE 1.17.0.
When adding FreeRTOS support to my project, the program hangs soon after osKernelStart() is called.
I had hard time finding the culprit.

The problem is that the SysTick_Handler() present in cmsis_os2.c is not used (It is surrounded with #if defined(SysTick) /  #endif).
Because os this, the default handler is called (infinite while loop).

I've worked around this problem by copying the SysTick_Handler() function in my code. But this problem should be fixed in the STM32CubeIDE code generator.

Best regards,

Nicolas

This topic has been closed for replies.

4 replies

ST Technical Moderator
Dec 13, 2024 3:05 PM UTC

Hello @DrPiWork 

Make sure to use the STM32CubeMX version 6.13.0.

If the issue is not resolved with this latest release, please share your ioc file to reproduce this.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
DrPiWorkAuthor
Associate II
Dec 17, 2024 8:06 AM UTC

Hello,

I'm using STM32CubeIDE 1.17.0.

From what I can see in the Help / Installation details / Installed software menu, it uses STM32CubeMX 6.13.0.202411220809

Regards,
Nicolas

 

DrPiWorkAuthor
Associate II
Dec 17, 2024 9:10 AM UTC

I forgot the .ioc file. Here it is.

Nicolas

vas
Associate
Feb 18, 2025 4:49 PM UTC

It looks like I have a similar issue here. Could you please tell if this was fixed already?