Skip to main content
Javier1
Principal
February 11, 2021
Solved

Flashing empty memory pages with cubemx locks my mcu

Good evening stm32 dwellings, i have a flash problem.

I find myself with the need to write a config file independent to my programm code.

In order to do that my programm uses pointers to specific memory pages of my stm32f105:

define ADDR_FLASH_PAGE_54 ((uint32_t)0x0801B000) /* Base @ of Page 54, 2 Kbytes */
#define ADDR_FLASH_PAGE_55 ((uint32_t)0x0801B800) /* Base @ of Page 55, 2 Kbytes */

For debugging purposes i created a temporal setup function that writes the a hardcoded config structure directly to my flash. (<- this is working fine, reading and writting)

BUT

Once i build my own configFile.bin and try to flash it with stm32cubeMX i get this:

 0693W000007EwP0QAK.png 

the flashed data looks fine when i read the memory, but the mcu is locked, once i start a debugging session it goes into hardfault at random moments.

this is the verbosity output of the stm32cubeMX flashing

I have no idea of what is going on....

16:38:55:746 : Memory Programming ...
 16:38:55:756 : Opening and parsing file: archivobinario_pointerArray.bin
 16:38:55:757 : File : archivobinario_pointerArray.bin
 16:38:55:757 : Size : 120 Bytes
 16:38:55:757 : Address : 0x0801B000 
 16:38:55:757 : Erasing Segment <0> Address <0x0801B000> Size <120>Bytes
 16:38:55:758 : Erasing memory corresponding to segment 0:
 16:38:55:760 : Memory erase...
 16:38:55:760 : halt ap 0 
 16:38:55:760 : w ap 0 reg 15 PC (0x20000000) 
 16:38:55:760 : w ap 0 reg 17 MSP (0x20000500) 
 16:38:55:760 : w ap 0 reg 16 xPSR (0x01000000) 
 16:38:55:763 : w ap 0 @0x20000960 0x00000200 bytes Data 0x00000000
 16:38:55:767 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
 16:38:55:783 : w ap 0 @0x20000004 0x0000053E bytes Data 0xF000B580
 16:38:55:790 : Erasing internal memory sector 54
 16:38:55:791 : Init flashloader...
 16:38:55:792 : halt ap 0 
 16:38:55:792 : w ap 0 reg 0 R0 0x00000001
 16:38:55:793 : w ap 0 reg 1 R1 0x00000000
 16:38:55:793 : w ap 0 reg 2 R2 0x00000000
 16:38:55:793 : w ap 0 reg 3 R3 0x00000000
 16:38:55:793 : w ap 0 reg 4 R4 0x00000000
 16:38:55:794 : w ap 0 reg 5 R5 0x00000000
 16:38:55:795 : w ap 0 reg 6 R6 0x00000000
 16:38:55:795 : w ap 0 reg 7 R7 0x00000000
 16:38:55:795 : w ap 0 reg 8 R8 0x00000000
 16:38:55:796 : w ap 0 reg 9 R9 0x00000000
 16:38:55:797 : w ap 0 reg 10 R10 0x00000000
 16:38:55:798 : w ap 0 reg 11 R11 0x00000000
 16:38:55:799 : w ap 0 reg 12 R12 0x00000000
 16:38:55:804 : w ap 0 reg 13 SP 0x00000000
 16:38:55:805 : w ap 0 reg 14 LR 0x20000001
 16:38:55:805 : w ap 0 reg 15 PC 0x20000005
 16:38:55:805 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:805 : w ap 0 reg 17 MSP 0x2000093E
 16:38:55:805 : w ap 0 reg 18 PSP 0x00000000
 16:38:55:805 : run ap 0 
 16:38:55:806 : halt ap 0 
 16:38:55:806 : r ap 0 reg 0 R0 0x00000001
 16:38:55:806 : Loader sector erase...
 16:38:55:806 : w ap 0 reg 0 R0 0x0801B000
 16:38:55:806 : w ap 0 reg 1 R1 0x0801B000
 16:38:55:808 : w ap 0 reg 2 R2 0x00000002
 16:38:55:808 : w ap 0 reg 3 R3 0x00000000
 16:38:55:808 : w ap 0 reg 4 R4 0x00000000
 16:38:55:808 : w ap 0 reg 5 R5 0x00000000
 16:38:55:808 : w ap 0 reg 6 R6 0x00000000
 16:38:55:808 : w ap 0 reg 7 R7 0x00000000
 16:38:55:808 : w ap 0 reg 8 R8 0x00000000
 16:38:55:808 : w ap 0 reg 9 R9 0x00000000
 16:38:55:809 : w ap 0 reg 10 R10 0x00000000
 16:38:55:809 : w ap 0 reg 11 R11 0x00000000
 16:38:55:809 : w ap 0 reg 12 R12 0x00000000
 16:38:55:809 : w ap 0 reg 13 SP 0x00000000
 16:38:55:809 : w ap 0 reg 14 LR 0x20000001
 16:38:55:810 : w ap 0 reg 15 PC 0x200001AF
 16:38:55:812 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:812 : w ap 0 reg 17 MSP 0x2000093E
 16:38:55:813 : w ap 0 reg 18 PSP 0x00000000
 16:38:55:813 : run ap 0 
 16:38:55:868 : halt ap 0 
 16:38:55:868 : r ap 0 reg 0 R0 0x00000001
 16:38:55:868 : erase: 0069ms
 16:38:55:869 : Download in Progress:
 16:38:55:869 : Size : 120 Bytes
 16:38:55:869 : Address : 0x0801B000 
 16:38:55:869 : Buffer program...
 16:38:55:870 : halt ap 0 
 16:38:55:870 : w ap 0 reg 15 PC (0x20000000) 
 16:38:55:870 : w ap 0 reg 17 MSP (0x20000500) 
 16:38:55:870 : w ap 0 reg 16 xPSR (0x01000000) 
 16:38:55:871 : w ap 0 @0x20000960 0x00000200 bytes Data 0x00000000
 16:38:55:871 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
 16:38:55:877 : w ap 0 @0x20000004 0x0000053E bytes Data 0xF000B580
 16:38:55:877 : Loader write range...
 16:38:55:878 : w ap 0 @0x20000960 0x0000003C bytes Data 0x0801B800
 16:38:55:878 : W B1 in RAM @0x20000960 size 0x0000003C : 0002ms
 16:38:55:878 : Init flashloader...
 16:38:55:878 : halt ap 0 
 16:38:55:878 : w ap 0 reg 0 R0 0x00000001
 16:38:55:878 : w ap 0 reg 1 R1 0x00000000
 16:38:55:879 : w ap 0 reg 2 R2 0x00000000
 16:38:55:879 : w ap 0 reg 3 R3 0x00000000
 16:38:55:879 : w ap 0 reg 4 R4 0x00000000
 16:38:55:879 : w ap 0 reg 5 R5 0x00000000
 16:38:55:879 : w ap 0 reg 6 R6 0x00000000
 16:38:55:879 : w ap 0 reg 7 R7 0x00000000
 16:38:55:879 : w ap 0 reg 8 R8 0x00000000
 16:38:55:879 : w ap 0 reg 9 R9 0x00000000
 16:38:55:880 : w ap 0 reg 10 R10 0x00000000
 16:38:55:880 : w ap 0 reg 11 R11 0x00000000
 16:38:55:880 : w ap 0 reg 12 R12 0x00000000
 16:38:55:881 : w ap 0 reg 13 SP 0x00000000
 16:38:55:882 : w ap 0 reg 14 LR 0x20000001
 16:38:55:882 : w ap 0 reg 15 PC 0x20000005
 16:38:55:883 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:884 : w ap 0 reg 17 MSP 0x2000093E
 16:38:55:887 : w ap 0 reg 18 PSP 0x00000000
 16:38:55:887 : run ap 0 
 16:38:55:887 : halt ap 0 
 16:38:55:887 : r ap 0 reg 0 R0 0x00000001
 16:38:55:888 : w ap 0 reg 0 R0 0x0801B000
 16:38:55:888 : w ap 0 reg 1 R1 0x0000003C
 16:38:55:888 : w ap 0 reg 2 R2 0x20000960
 16:38:55:888 : w ap 0 reg 3 R3 0x00000002
 16:38:55:888 : w ap 0 reg 4 R4 0x00000000
 16:38:55:889 : w ap 0 reg 5 R5 0x00000000
 16:38:55:889 : w ap 0 reg 6 R6 0x00000000
 16:38:55:890 : w ap 0 reg 7 R7 0x00000000
 16:38:55:890 : w ap 0 reg 8 R8 0x00000000
 16:38:55:890 : w ap 0 reg 9 R9 0x00000000
 16:38:55:890 : w ap 0 reg 10 R10 0x00000000
 16:38:55:890 : w ap 0 reg 11 R11 0x00000000
 16:38:55:891 : w ap 0 reg 12 R12 0x00000000
 16:38:55:891 : w ap 0 reg 13 SP 0x00000000
 16:38:55:891 : w ap 0 reg 14 LR 0x20000001
 16:38:55:891 : w ap 0 reg 15 PC 0x2000002F
 16:38:55:891 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:891 : w ap 0 reg 17 MSP 0x2000093E
 16:38:55:891 : w ap 0 reg 18 PSP 0x00000000
 16:38:55:891 : run ap 0 
 16:38:55:892 : w ap 0 @0x2000099C 0x0000003C bytes Data 0x0801B800
 16:38:55:892 : W B2 in RAM @0x20008360 size 0x0000003C: 0027ms
 16:38:55:892 : r ap 0 reg 0 R0 0x00000001
 16:38:55:892 : Wait W B1 in Flash @0x0801B000 size 0x0000003C: 0001ms
 16:38:55:893 : w ap 0 reg 0 R0 0x0801B03C
 16:38:55:893 : w ap 0 reg 1 R1 0x0000003C
 16:38:55:894 : w ap 0 reg 2 R2 0x2000099C
 16:38:55:894 : w ap 0 reg 3 R3 0x00000002
 16:38:55:894 : w ap 0 reg 4 R4 0x00000000
 16:38:55:894 : w ap 0 reg 5 R5 0x00000000
 16:38:55:895 : w ap 0 reg 6 R6 0x00000000
 16:38:55:895 : w ap 0 reg 7 R7 0x00000000
 16:38:55:896 : w ap 0 reg 8 R8 0x00000000
 16:38:55:897 : w ap 0 reg 9 R9 0x00000000
 16:38:55:898 : w ap 0 reg 10 R10 0x00000000
 16:38:55:899 : w ap 0 reg 11 R11 0x00000000
 16:38:55:899 : w ap 0 reg 12 R12 0x00000000
 16:38:55:901 : w ap 0 reg 13 SP 0x00000000
 16:38:55:901 : w ap 0 reg 14 LR 0x20000001
 16:38:55:903 : w ap 0 reg 15 PC 0x2000002F
 16:38:55:903 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:903 : w ap 0 reg 17 MSP 0x2000093E
 16:38:55:903 : w ap 0 reg 18 PSP 0x00000000
 16:38:55:903 : run ap 0 
 16:38:55:904 : r ap 0 reg 0 R0 0x00000001
 16:38:55:904 : Write elapsed time: 0042ms
 16:38:55:904 : Segment[0] downloaded successfully
 16:38:55:905 : File download complete
 16:38:55:924 : Time elapsed during download operation: 00:00:00.130
 16:38:55:924 : RUNNING Program ... 
 16:38:55:924 : Address: : 0x0801B000
 16:38:55:934 : w ap 0 reg 15 PC 0x0801B858
 16:38:55:936 : w ap 0 reg 17 MSP 0x0801B800
 16:38:55:939 : w ap 0 reg 16 xPSR 0x01000000
 16:38:55:940 : Warning: The core is locked up
 16:38:55:954 : Start operation achieved successfully

Extra ball: if i do full chip erase and then i flash again my small config file at start address 0x0801B000 i also get the Warning: The core is locked up

This topic has been closed for replies.
Javier1
Javier1Best answer
Principal
April 24, 2023

I did overcome this issue purely by ignoring It.

I Believe the core is locked Up message showed Up because cubeprogrammer was tryingto run the binary file right after flashing.

​

As It was just raw config data not compiled Code , thus it was crashing​

hit me up in https://www.linkedin.com/in/javiermuñoz/

2 replies

CCend.2
Associate II
April 24, 2023

I'm having the same issue when flashing my chip using STM32CubeProgrammer. Were you ever able to fix it?

Javier1
Javier1AuthorBest answer
Principal
April 24, 2023

I did overcome this issue purely by ignoring It.

I Believe the core is locked Up message showed Up because cubeprogrammer was tryingto run the binary file right after flashing.

​

As It was just raw config data not compiled Code , thus it was crashing​

hit me up in https://www.linkedin.com/in/javiermuñoz/