Skip to main content
KK.2
Associate II
Aug 25, 2020 8:17 PM UTC
Solved

[Fixed] Cant get ADC to work

Trying to read out a resistive touchscreen right now. To keep everything as simple as possible for testing I created an empty project in CubeMX just for testing this and set up all the pins in a static fashion (No reconfiguration at runtime)

Measuring the ADC input with a multimeter I correctly see the voltage depending on where I touch, however no matter what I try, the ADC always either outputs a static number (Usually the max value of my configured resolution) or at random will (E.g. with 10 bit) Output a value like 0, 255, 512 or 1024.

To eliminate the variable of the touchscreen I've also tried to remove the Touchscreen and connect a potentiometer directly which is connected between ground and 3v3 which made no difference.

I tried pretty much all combinations of resolutions, sample times, Interrupt or not, its always the same result. I have also tried to use ADC2 / ADC3 instead of ADC1 with the same result.

My code looks like this:

HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);
uint16_t xpos = HAL_ADC_GetValue(&hadc1);
HAL_ADC_Stop(&hadc1);

Continuous conversion is enabled, leaving out the ADC Stop makes no difference. I pretty much have no idea any more, if somebody can help me that would be appreciated.

This topic has been closed for replies.
KK.2
KK.2Best answer
Associate II
Aug 25, 2020 9:36 PM UTC

Like I've said, Ive tested a lot of things, different values for `HAL_MAX_DELAY` is one of them, regardless in my case it is a hardware issue as vref+ was not connected to vdd / vdda due to poor soldering. Having corrected that it is now working.

2 replies

LMI2
Senior III
Aug 25, 2020 9:20 PM UTC

Several people have posted working ADC code. If you search for instance HAL_ADC_PollForConversion

you'll get a working examples elswhere, too. I wonder why you use HAL_MAX_DELAY, what I remeber 1000 or so is enough. And Where is Getvalue command, I have used that. This may have worked, it is old code, so I'm not 100% sure.

 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
		//K15_Pin|K1_Pin|K3_Pin|K16_Pin
		HAL_GPIO_TogglePin(GPIOD,K16_Pin);
		HAL_GPIO_TogglePin(GPIOD,K15_Pin);
		HAL_GPIO_TogglePin(GPIOD,K1_Pin);
		HAL_GPIO_TogglePin(GPIOD,K3_Pin);
 
	while	(HAL_ADC_PollForConversion(&hadc1,0)!=HAL_OK)
	{
luku=HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_4);//
luku=HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_5);//
luku=HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_6);//
luku=HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_7);//		
	}
luku = HAL_ADC_GetValue(&hadc1);
		sprintf(msg ,"Welcome %d",luku);
HAL_UART_Transmit(&huart1, (uint8_t*)msg, strlen(msg), 1000);
		HAL_ADC_Stop(&hadc1);
	HAL_ADC_Start(&hadc1);
		HAL_Delay(5000);
 }

KK.2
KK.2AuthorBest answer
Associate II
Aug 25, 2020 9:36 PM UTC

Like I've said, Ive tested a lot of things, different values for `HAL_MAX_DELAY` is one of them, regardless in my case it is a hardware issue as vref+ was not connected to vdd / vdda due to poor soldering. Having corrected that it is now working.