Skip to main content
koendv
Associate II
May 19, 2026 9:06 AM UTC
Solved

Feature request: Wildcard support in STM32CubeMX pin/signal search

Hello,

I would like to request an enhancement to the search functionality in STM32CubeMX's pinout view.

Currently, the search works well for exact or partial matches — for example, typing "usart1_rx" highlights the relevant pins. However, it would be very useful to support wildcard characters, allowing searches such as:

- usart?_rx — match RX pins across all USART peripherals (USART1, USART2, etc.)
- usart1_?x — match both RX and TX on USART1
- *art*_?x — match all RX and TX signals on LPUART, UART, USART

This would be especially helpful on larger packages with many peripherals, where you want to quickly visualize all pins serving a particular role across multiple instances of the same peripheral.

The implementation complexity should be low — this is essentially replacing the existing string match with a simple wildcard pattern matcher against the same search index.

Thank you for considering this improvement!

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 19, 2026 9:25 AM UTC

This function already exists anyway - you just need to type, for example, USART1_*X into the search field and all the relevant pins will start blinking, even a wildcard like ?? or ? instead of * works?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 19, 2026 9:25 AM UTC

This function already exists anyway - you just need to type, for example, USART1_*X into the search field and all the relevant pins will start blinking, even a wildcard like ?? or ? instead of * works?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.