Skip to main content
Visitor
Nov 2, 2026 11:08 AM UTC
Question

Feature Request – Compile-Time Register-Level Code Generation for STM32CubeMX / CubeMX2

Dear STMicroelectronics Development Team,

I would like to suggest a feature that could significantly improve STM32CubeMX and STM32CubeMX2, particularly for embedded projects with limited Flash memory and strict performance requirements.

Current Situation

When configuring peripherals such as GPIO, timers, ADC, UART, SPI, etc., CubeMX typically generates initialization code using HAL or LL functions.

Although these libraries provide a convenient and structured programming interface, the generated initialization code can introduce considerable overhead.

In many cases, the hardware configuration is completely static and known at compile time. However, the generated code may still involve multiple function calls, intermediate structures, parameter assignments, and runtime operations just to write a few fixed values into hardware registers.

For example, configuring a GPIO port might ultimately require only a few register writes with constant values. Yet the generated initialization code can be considerably larger than the actual hardware configuration requires.

This becomes particularly problematic in memory-constrained applications, where even initialization code contributes to Flash consumption.

Proposed Feature: Direct Register-Level Code Generation

I suggest adding an optional code-generation backend that converts the selected CubeMX configuration directly into optimized register-level initialization code.

Instead of generating HAL/LL initialization functions, CubeMX could calculate all required register values during code generation and produce a minimal C implementation using constant values.

For example, instead of generating multiple HAL calls and configuration structures, the output could be equivalent to:

void GPIO_Init(void)
{
RCC->AHB2ENR |= 0x00000001UL;

GPIOA->MODER = 0x........UL;
GPIOA->OTYPER = 0x........UL;
GPIOA->OSPEEDR = 0x........UL;
GPIOA->PUPDR = 0x........UL;
GPIOA->AFR[0] = 0x........UL;
}

The actual values would be calculated by CubeMX based on the user's configuration.

With constant values and suitable compiler optimization, the resulting assembly could be reduced to a very small number of direct register-write instructions, without unnecessary runtime calculations or function calls.

Suggested Implementation

Rather than replacing HAL or LL, this could be offered as an additional code-generation option:

  1. HAL-based generation (existing functionality).

  2. LL-based generation (existing functionality).

  3. Direct Register-Level generation (new option).

The new option should:

  • Calculate register values during code generation, not at runtime.

  • Generate direct register writes using compile-time constants.

  • Avoid unnecessary initialization structures and function calls.

  • Generate only the registers and operations required by the selected configuration.

  • Respect register-specific behavior, including reserved bits, write-one-to-clear flags, and required initialization sequences.

  • Support all applicable STM32 families, not just newly introduced families.

Ideally, users should be able to select this generation method independently for each peripheral.

Expected Benefits

  • Significantly reduced initialization code size.

  • Lower Flash consumption.

  • Faster system startup.

  • Reduced runtime overhead.

  • No dependency on HAL or LL for the generated initialization code.

  • Better suitability for resource-constrained embedded applications.

  • Greater control over the final machine code.

An Additional Benefit

CubeMX already has all the necessary information about pin assignments, clock configuration, peripheral modes, and register settings.

Therefore, it should be possible to calculate the final register values internally without requiring the user to manually inspect generated code, debug initialization functions, or extract register values.

This would also reduce human errors associated with manually translating HAL configurations into register-level code.

I believe this feature would be valuable not only for advanced embedded developers but also for applications where code size, startup time, and execution efficiency are critical.

Thank you for considering this suggestion.

Best regards

5 replies

Ghofrane GSOURI
ST Technical Moderator
Nov 2, 2026 1:32 PM UTC

Hello ​@pf_55 

Thank you for your detailed suggestion and for highlighting the needs of memory-constrained applications.

STMicroelectronics has invested significantly in HAL and LL to provide supported, maintainable peripheral drivers across the STM32 portfolio. HAL prioritizes portability and ease of integration, while LL provides interfaces closer to the hardware for applications requiring finer control and lower overhead.

For the use case you describe, LL is the existing option most closely aligned with your objectives. Depending on the peripheral and device, LL offers inline register-access functions that, with constant arguments and compiler optimization, can produce compact code. 

Introducing a separate direct-register backend would require an additional code-generation path to be developed, validated, and maintained across supported devices. It would still need to respect device-specific register behavior and initialization sequences, while ensuring compatibility with the application’s drivers and middleware.

Given the investment in HAL and LL, improving the efficiency of existing LL-based generation would be a more practical direction to evaluate than introducing a third backend with its own ongoing validation and maintenance requirements.

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TDK
Nov 2, 2026 2:41 PM UTC

ST has consistently denied this request. Back when we could vote on suggestions, this was the #1 highest voted suggestion.

The answer to “library with less overhead” has been LL and HAL2.

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
Nov 2, 2026 3:51 PM UTC

In other words, if you want register access programming, simply avoid using Cube/CubeMX. There’s no support from ST for that, though, and they are stubborn in this for years.

May be fine as a graphical tool to assign pins, though (that was the original aim of the MicroXplorer, from which CubeMX evolved).

JW

gbm
Super User
Nov 3, 2026 7:34 AM UTC

Well, I did that few years ago - defined some useful data structures and macros for use in all my STM32 projects. The next step should be the pull-down list-driven generation of code using (maybe) a spreadsheet. The data structures I use may be found here:

https://github.com/gbm-ii/STM32_Inc/blob/main/bf_reg.h

And here is a sample of code using them:

// the whole port init
GPIOB->AFR[0] = (union bf4_) {
.p0 = 2, // TIM3CH3 INJ2
.p4 = 8, // I2C2 SDA
.p5 = 8, // I2C2 SCL
}.w;
GPIOB->AFR[1] = (union bf4_) {
.p12 = 5, // SPI2 NSS2A - PT2
.p13 = 5, // SPI2 SCK
.p14 = 5, // SPI2 MISO
.p15 = 5, // SPI2 MOSI
}.w;
GPIOB->OSPEEDR = (union bf2_) {
.p4 = GPIO_OSPEEDR_MED, // I2C2_SDA
.p5 = GPIO_OSPEEDR_MED, // I2C2_SCL
.p12 = GPIO_OSPEEDR_HI,
.p13 = GPIO_OSPEEDR_HI,
.p14 = GPIO_OSPEEDR_HI,
.p15 = GPIO_OSPEEDR_HI,
}.w;

GPIOB->MODER = (union bf2_) {
.p0 = GPIO_MODER_AF, // INJ2
.p1 = GPIO_MODER_AN, // nc
.p2 = GPIO_MODER_AN, // nc
.p3 = GPIO_MODER_AN, // nc
.p4 = GPIO_MODER_AF, // SDA
.p5 = GPIO_MODER_AF, // SCL
.p6 = GPIO_MODER_AN, // nc
.p7 = GPIO_MODER_AN, // nc
.p8 = GPIO_MODER_AN, // button
.p9 = GPIO_MODER_AN, // no pin
.p10 = GPIO_MODER_AN, // nc
.p11 = GPIO_MODER_AN, // no pin
.p12 = GPIO_MODER_OUT , // NSS2A
.p13 = GPIO_MODER_AF, // SCK2
.p14 = GPIO_MODER_AF, // MISO
.p15 = GPIO_MODER_AF, // MOSI
}.w;

// selected port lines init
RCC->IOENR |= RCC_IOENR_GPIOEN(GPIOA);
AFRF(GPIOA, 11) = AFN_USB;
AFRF(GPIOA, 12) = AFN_USB;
BF2F(GPIOA->OSPEEDR, 11) = GPIO_OSPEEDR_HI;
BF2F(GPIOA->OSPEEDR, 12) = GPIO_OSPEEDR_HI;
BF2F(GPIOA->MODER, 11) = GPIO_MODER_AF;
BF2F(GPIOA->MODER, 12) = GPIO_MODER_AF;

 

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Pavel A.
Nov 3, 2026 11:08 PM UTC

>  The next step should be the pull-down list-driven generation of code using (maybe) a spreadsheet. 

These days: an AI agent with appropriate skill script(s).