Skip to main content
Associate III
Nov 19, 2026 4:51 PM UTC
Question

FDCAN Clock Mux Code Gen Doesn't Work For PLL2Q

Hello,

I’m using STM32Cube FW_H7 V1.9.1 and CubeMX  6.8.1-RC4 for STM32H723ZGTx

In Clock Configuration, if I select PLL1Q, FDCANSEL = 1.

 

 

However, if I select PLL2Q, FDCANSEL = 0 when it should be 2.

 

The cause seems to be missing generated code when PLL2Q is selected:

 

 

Is this a code generator problem or a mistake I’ve made please?

1 reply

TDK
Nov 19, 2026 6:43 PM UTC

Probably the same bug as here:

No updates since it was acknowledged 11 months ago. Could be resolved however.

CubeMX  6.8.1-RC4

A 3 year old version? Latest version is 6.19. Does it work there?

"If you feel a post has answered your question, please click ""Accept as Solution""."