Skip to main content
Visitor II
July 11, 2025
Question

Failed in update the firmware package for STM32H5

I download the latest firmware package "stm32cubeh5-v1-5-0.zip" for STM32H5, from ST's website. I followed following instructions to install it via STM32CubeMX:

  • Open STM32CubeMX. 
     
  • Go to Help > Manage embedded software packages. 
     
  • Choose the desired STM32Cube MCU Package for your specific series (e.g., STM32CubeL4 for STM32L4 series). 
     
  • Click "Install" or "From Local" if you have a downloaded archive. 
     
  • The firmware and examples will be installed in the STM32Cube repository, usually under C:\Users\<your_username>\STM32Cube\Repository. 

 I get following failure message, at the very end of the installation process:

WenLiu_0-1752236346137.png

I checked the Repository directory, The previous version - "STM32Cube_FW_H5_V1.3.0" is installed. Should I uninstall the V1.3.0 first, before I can install V1.5.0?

Any helps? Thanks!

 

This topic has been closed for replies.

2 replies

TDK
July 11, 2025

Renaming the existing directory temporarily would let you find out if it's the problem without installing.

 

Installing via Help -> Manage Embedded... is the more supported option.

TDK_0-1752238902506.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Semer CHERNI
ST Employee
July 11, 2025

Hello @Wen-Liu 

First let me thank you for posting.

I was able to install STM32Cube_FW_H5_V1.5.0 while having STM32Cube_FW_H5_V1.3.0.

Could you check the STM32Cube\Repository?

BR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.