Skip to main content
MKosc.1
Associate
February 24, 2023
Solved

Examples not accessible in CubeMX for NUCLEO-L031K6?

Hello,

I was trying to setup a prototyping project using the NUCLEO-L031K6 examples. But the current CubeMX version 6.7.0 does not seem so know about this dev board at all.

Is this a bug or is this nucleo board not fully supported by CubeMX?

This topic has been closed for replies.
Foued_KH
Foued_KHBest answer
ST Employee
February 24, 2023

Hello @MKosc.1​ ,

Not All STM32 MCUs have examples with .ioc file in the Cube FW and STM32CubeMX don't provides examples for all MCUs.

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

Peter BENSCH
ST Technical Moderator
February 24, 2023

Welcome, @MKosc.1​, to the community!

It is not a bug, the board is visible - at least on my machine. :grinning_face:

Have you installed the embedded software packages for the STM32L4?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Foued_KH
Foued_KHBest answer
ST Employee
February 24, 2023

Hello @MKosc.1​ ,

Not All STM32 MCUs have examples with .ioc file in the Cube FW and STM32CubeMX don't provides examples for all MCUs.

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MKosc.1
MKosc.1Author
Associate
February 24, 2023

Hello,

thank you for the very fast replies! I seem to have misphrased the issue - the board is indeed visible as Peter pointed out and I can start a project based on it.

I just assumed the examples with associated .ioc files are commonly provided as well for all ST dev boards - thank you for pointing that out to me Foued.

I will proceed with the available configuration, just wanted to be sure I'm not missing something :)

Foued_KH
ST Employee
February 24, 2023

yes sure you can share your project with me :D

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.