Skip to main content
Kendric RUIZ
Associate
Apr 6, 2017 11:14 AM UTC
Question

Ethernet-TCPip Nucleo F429ZIT6

Posted on April 06, 2017 at 13:14

Hi,

I use STM32CubeMX to generate t

he configuration of LWip on my card (nucleo F429ZIT6).

Once my card program, I address a fixed IP address but I can't see my card on the local networks.

The code generated is :

int main()

{

   HAL_INIT();

   SystemClock_Config();

   MX_LWIP_INIT();

   While(1);

}

I have no mistake, should I be able to ping my card?

Thank !

#tcp/ip #lwip #ethernet #cubemx #stm32f4
This topic has been closed for replies.

2 replies

ST Technical Moderator
Apr 6, 2017 1:02 PM UTC
Posted on April 06, 2017 at 15:02

Hi

kendric.ruiz

,

You find many examples ready-to-user with

STM32CubeF4

at this path that can help you on your project and you may re-use sections available in the examples or get inspired from them: STM32Cube_FW_F4_V1.0\Projects\STM32469I_EVAL\Applications\LwIP

- AN3966 : “LwIP TCP/IP stack demonstration for STM32F4x7 microcontrollers�?

- UM1713 : “Developing applications on STM32Cube with LwIP TCP/IP stack�?

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Kendric RUIZ
Associate
Apr 6, 2017 3:24 PM UTC
Posted on April 06, 2017 at 15:24

Thanks a lot !

Kendric