Skip to main content
Taco!
Visitor II
Nov 27, 2019 7:07 PM UTC
Question

Error[Lp015]: section placement failure caused by HAL_Unlock???

Im using an F4 and modified my code to support an analog input using CubeMX. It messed up my project directory so i copied the new adc files to my unharmed project. I now get an "Error[Lp015]: section placement failure: overcommitted content in [0x802'0000-0x803'ffff]" and "Error while running Linker".

Part of the code in the auto generated adc.c file is a function called MX_ADC1_Init();

If i call this function i get the above error. If it is commented out, it builds successfully. If i call that function but comment everything out it builds successfully. If I incrementally add things in until i get the error then it fails within the HAL_ADC_Init() function (which is within the MX_ADC1_Init() function). Within the HAL_ADC_Init() function it fails when I uncomment hadc->Lock = HAL_UNLOCKED;

The code below shows the hadc->Lock = HAL_UNLOCKED as uncommented. Has anyone seen this before? What could cause it? How do I fix it?

Edit: worth noting is that many other unlock statements work correctly (ie: huart->Lock = HAL_UNLOCK, htim->Lock = ..., heth, hspi, hi2c, hrng, etc.)

HAL_StatusTypeDef HAL_ADC_Init(ADC_HandleTypeDef* hadc)
{
 HAL_StatusTypeDef tmp_hal_status = HAL_OK;
// 
// /* Check ADC handle */
 if(hadc == NULL)
 {
 return HAL_ERROR;
 }
// 
// /* Check the parameters */
 assert_param(IS_ADC_ALL_INSTANCE(hadc->Instance));
 assert_param(IS_ADC_CLOCKPRESCALER(hadc->Init.ClockPrescaler));
 assert_param(IS_ADC_RESOLUTION(hadc->Init.Resolution));
 assert_param(IS_FUNCTIONAL_STATE(hadc->Init.ScanConvMode));
 assert_param(IS_FUNCTIONAL_STATE(hadc->Init.ContinuousConvMode));
 assert_param(IS_ADC_EXT_TRIG(hadc->Init.ExternalTrigConv));
 assert_param(IS_ADC_DATA_ALIGN(hadc->Init.DataAlign));
 assert_param(IS_ADC_REGULAR_LENGTH(hadc->Init.NbrOfConversion));
 assert_param(IS_FUNCTIONAL_STATE(hadc->Init.DMAContinuousRequests));
 assert_param(IS_ADC_EOCSelection(hadc->Init.EOCSelection));
 assert_param(IS_FUNCTIONAL_STATE(hadc->Init.DiscontinuousConvMode));
// 
 if(hadc->Init.ExternalTrigConv != ADC_SOFTWARE_START)
 {
 assert_param(IS_ADC_EXT_TRIG_EDGE(hadc->Init.ExternalTrigConvEdge));
 }
// 
 if(hadc->State == HAL_ADC_STATE_RESET)
 {
// /* Initialize ADC error code */
 ADC_CLEAR_ERRORCODE(hadc);
// 
// /* Allocate lock resource and initialize it */
 hadc->Lock = HAL_UNLOCKED; //THIS IS THE FAILURE POINT!!!!!!!!!!!!
// 
// /* Init the low level hardware */
// HAL_ADC_MspInit(hadc);
 }
// 
// /* Configuration of ADC parameters if previous preliminary actions are */ 
// /* correctly completed. */
// if (HAL_IS_BIT_CLR(hadc->State, HAL_ADC_STATE_ERROR_INTERNAL))
// {
// /* Set ADC state */
// ADC_STATE_CLR_SET(hadc->State,
// HAL_ADC_STATE_REG_BUSY | HAL_ADC_STATE_INJ_BUSY,
// HAL_ADC_STATE_BUSY_INTERNAL);
// 
// /* Set ADC parameters */
// ADC_Init(hadc);
// 
// /* Set ADC error code to none */
// ADC_CLEAR_ERRORCODE(hadc);
// 
// /* Set the ADC state */
// ADC_STATE_CLR_SET(hadc->State,
// HAL_ADC_STATE_BUSY_INTERNAL,
// HAL_ADC_STATE_READY);
// }
// else
// {
// tmp_hal_status = HAL_ERROR;
// }
// 
// /* Release Lock */
// __HAL_UNLOCK(hadc);
 
 /* Return function status */
 return tmp_hal_status;
}

This topic has been closed for replies.

4 replies

Pavel A.
Nov 28, 2019 12:25 AM UTC

> overcommitted content in [0x802'0000-0x803'ffff]"

So, is the program just growing more than 128K?

-- pa

Ozone
Principal
Nov 28, 2019 6:49 AM UTC

I agree - ssupposedly your code size grew beyond Flash size.

Check the linker map file, to see which objects seize that much space.

Piranha
Principal III
Nov 28, 2019 6:37 PM UTC

AMap - a nice tool to look at *.map files.

Pavel A.
Nov 28, 2019 7:37 PM UTC

Atollic and Cube IDE have a similar tool, the Build Analyzer.

Open it after successful build. For best results, check "generate list file" in post-build outputs.

-- pa