Skip to main content
Dmitri
Associate II
Nov 20, 2018 9:42 PM UTC
Question

Error downloading FW.F1.1.7.0 MCU package

Hi,

recently I installed STM32CubeMX. When I click 'Check for update' menu item 'STM32CubeF1 Firmware Package V1.7.0 / 09-October-2018' is shown. But when I press 'Install Now' the following error happens:

In the log I see:

2018-11-20 23:56:39,197 [ERROR] ServerAccessManage:919 - Problem, file not found on Server

2018-11-20 23:56:39,197 [ERROR] ServerAccessManage:491 - Problem, file not found on Server : stm32cube_fw_f1_v170.zip.

Is v1.7.0 package available to download?

thanks,

Dmitri

This topic has been closed for replies.

12 replies

Tesla DeLorean
Guru
Nov 20, 2018 10:15 PM UTC

ST looks to have got a bit ahead of themselves, issue from here also, expect it to be resolved shortly. ​ @Khouloud GARSI​ 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Khouloud GARSI
ST Employee
Nov 21, 2018 10:23 AM UTC

Hi @Dmitri​ ,

Issue confirmed from our side and highlighted internally.

Sorry for this inconvenience. This will be fixed ASAP!

Khouloud.

Houda GHABRI
ST Employee
Nov 21, 2018 11:40 AM UTC

Hello @Dmitri​ 

Thanks for your feedback.

FW F1 1.7.0 will be available Tomorrow after doing a refresh in update Manager.

Sorry for the inconvenience.

Best regards,

Houda

Khouloud GARSI
ST Employee
Nov 21, 2018 2:20 PM UTC

Hi @Dmitri​ ,

Issue solved: The STM32F1 v1.7.0 is now available for download.

Khouloud.

Tesla DeLorean
Guru
Nov 21, 2018 5:32 PM UTC

Confirmed, have it mirrored if anyone needs it, or the other releases. The F7.1.13.0 was 1.2GB!!

ST should really consider hosting torrents for those on lower bandwidth connections, download limits or those who have intermittent connections which might benefit from a restartable download, ie continue rather than start over...

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
fm_it
Associate
Nov 23, 2018 9:27 AM UTC

Still having this problem. Can you provide a mirror? Thanks

LOVEKUSH PRATAP
Associate II
Dec 21, 2018 4:17 AM UTC

I'm still getting this error

error downloading the following files: stm32cube_fw_f1_v170.zip(cannot unzip) stm32cubemx

Tesla DeLorean
Guru
Dec 21, 2018 4:23 AM UTC

Well the .ZIP should be in the Repository, you can Check/Test it with something like WinRAR.

More critically the system will fail this way if your hard drive is out of space. Figure you're going to need more than 3.6 GB free to download and unpack

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..