Skip to main content
Associate II
April 9, 2025
Question

Enabling Register Callback for Timer in CubeMX, when FreeRTOS is enabled generate incorrect code.

In my project I have FreeRTOS enabled, which occupies SysTick and Time increment is handled by TIM1. I also want to use basic timer as TIM6.
However, I don't want them both processed in weak redefined 

void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
Thus, I enabled register callback for TIM in CubeMX -> advance settings -> register callbacks.

The generated code appears in stm32f4xx_hal_timebase_tim.c and looks as following:
HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority)
{
 RCC_ClkInitTypeDef clkconfig;
 uint32_t uwTimclock = 0U;

 uint32_t uwPrescalerValue = 0U;
 uint32_t pFLatency;

 HAL_StatusTypeDef status;

 /* Enable TIM1 clock */
 __HAL_RCC_TIM1_CLK_ENABLE();

 /* Get clock configuration */
 HAL_RCC_GetClockConfig(&clkconfig, &pFLatency);

 /* Compute TIM1 clock */
 uwTimclock = 2*HAL_RCC_GetPCLK2Freq();

 /* Compute the prescaler value to have TIM1 counter clock equal to 1MHz */
 uwPrescalerValue = (uint32_t) ((uwTimclock / 1000000U) - 1U);

 /* Initialize TIM1 */
 htim1.Instance = TIM1;

 /* Initialize TIMx peripheral as follow:
 * Period = [(TIM1CLK/1000) - 1]. to have a (1/1000) s time base.
 * Prescaler = (uwTimclock/1000000 - 1) to have a 1MHz counter clock.
 * ClockDivision = 0
 * Counter direction = Up
 */
 htim1.Init.Period = (1000000U / 1000U) - 1U;
 htim1.Init.Prescaler = uwPrescalerValue;
 htim1.Init.ClockDivision = 0;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

 status = HAL_TIM_Base_Init(&htim1);
 if (status == HAL_OK)
 {
 /* Start the TIM time Base generation in interrupt mode */
 status = HAL_TIM_Base_Start_IT(&htim1);
 if (status == HAL_OK)
 {
 /* Enable the TIM1 global Interrupt */
 HAL_NVIC_EnableIRQ(TIM1_UP_TIM10_IRQn);
 /* Configure the SysTick IRQ priority */
 if (TickPriority < (1UL << __NVIC_PRIO_BITS))
 {
 /* Configure the TIM IRQ priority */
 HAL_NVIC_SetPriority(TIM1_UP_TIM10_IRQn, TickPriority, 0U);
 uwTickPrio = TickPriority;
 }
 else
 {
 status = HAL_ERROR;
 }
 }
 }

 HAL_TIM_RegisterCallback(&htim1, HAL_TIM_PERIOD_ELAPSED_CB_ID, TimeBase_TIM_PeriodElapsedCallback);

 /* Return function status */
 return status;
}

For some reason HAL_TIM_RegisterCallback() is called after HAL_TIM_Base_Start_IT(), which result's in setting custom callback, because Timer is already running. 
Moreover, the weak overwrite callback is still generated in main.c as following:

/**
 * @brief Period elapsed callback in non blocking mode
 * @note This function is called when TIM1 interrupt took place, inside
 * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment
 * a global variable "uwTick" used as application time base.
 * @PAram htim : TIM handle
 * @retval None
 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
 /* USER CODE BEGIN Callback 0 */

 /* USER CODE END Callback 0 */
 if (htim->Instance == TIM1)
 {
 HAL_IncTick();
 }
 /* USER CODE BEGIN Callback 1 */

 /* USER CODE END Callback 1 */
}

So it doesn't look correct, or a am I missing something?

 

 

 

This topic has been closed for replies.

2 replies

Ghofrane GSOURI
ST Technical Moderator
April 9, 2025

Hello @serg22 

First let me thank you posting.

I'm currently investigating this . I will get back to you asap.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ghofrane GSOURI
ST Technical Moderator
April 10, 2025

Hello @serg22 

Your contribution is much appreciated .
Issue has been raised to the development team for fix.

Internal ticket number : 207314 

I'll keep you posted on any updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.