Skip to main content
MRAFI.376
Associate
Oct 22, 2019 10:42 AM UTC
Question

Custom USB Device: "Unknown device (device descriptor request failed)" error in Windows

I'm using STM32L073RZ on my own board, and I am trying to program USB device (I tried virtual COM and HID, separately).But after plugging into PC it is detected (after a while) with "Unknown device (device descriptor request failed)" error in windows 1

Electrically (PCB):

I think that PCB is not an error here - I just have D+ and D- short tracks from the connector to the uC and that's all.

I have a pull-up 1.5k (I tried with and without it), but it is not even needed in STM32. I have check connection and a cable and I'm certain it connects.

 

Code:

I'm using HAL and STM32CubeMx generated code merged with my project

 

 

is this a software or hardware issue?

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Oct 22, 2019 2:38 PM UTC

If it is a part supporting the ROM System Loader, and USB DFU, try pulling BOOT0 high, and reset/connect as a DFU device, should report "STM32 in DFU Mode" or somesuch.

On your board make sure you're using a crystal oscillator, that it starts, and the speed and HSE_VALUE are consistent.

Try also on known hardware like an EVAL board, or LORA-DISCO board

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MRAFI.376
MRAFI.376Author
Associate
Oct 23, 2019 10:42 AM UTC

Thank you for your replay

I just try STM32 DFU USB class but it not working in STM32L073RZ nucleo board

why its not working in this development board?. I am using an external crystal oscillator of 8 MHz later i change usb clock configuration to 48 MHz internal USB clock but its not working

Later I use to STM32Cube L0 example code (USB CDC standalone application code for STM32L073Z eval board code) it is not working nucleo board

is this a Hardware or Software issue?

how do i solve this ?

I am using STM workbench as IDE

in Nucleo Boad VBUS is already connected to 3.3v through 0 ohm resistance ,I am not using any series resistance with D+ and D- line is there any issue with this Hardware configuration

I am also tried Ubuntu 18 os result is same as in windows OS

is there any Reference of USB hardware specifically for STM32L073Z nucleo development board

DCull.1
Associate
Feb 3, 2020 11:34 AM UTC

Hi,

I am also using the NUCLEO-L073RZ eval board and I am experiencing similar problems.

I create a USB CDC project with CubeMX and have connected a USB cable to pins 12 ,14 and 20 GND on the morpho connector CN10.

I also have not connected VBUS from the USB cable.

When I plug the USB cable in I get Device Descriptor Request Failedon my PC ( win 10 ).

I have ordered a different eval board (STM32L073Z-EVAL ) that has built in USB connector and a specific project for USB CDC on the peripheral, not through the ST-LINK USB. ( I hope !! ). Going to try to get this going then compare to L073RZ.

Regards.