VChap.2Visitor II5 years agoMay 27, 2021 12:28 PM UTCQuestionCubeMX v6.2.1 + FreeRTOS v10.0.1 package + "Use FW pack heap file" option: Bug when generate Makefile0 replies633 viewsIn my project I want to use custom heap functions.To do this, I set the "Use FW pack heap file" option in the FreeRTOS settings, to "Disable".Despite this, the code generator still adds the package heap file (heap_4.c) to the list of files to compile.When linking a project, it conflicts with the custom memory allocation functions in my project.Cube is v6.2.1 (with last updates), FreeRTOS v10.0.1A bug demonstration project is in the attachmentbug_demonstration.7zSTM32CubeMXBug-reportFreeRTOS