Skip to main content
Associate
May 10, 2026 3:36 PM UTC
Question

CubeMX STM32WB55 linker file problem?

Hi, can someone please check what is wrong here: 

CubeMX/CubeIDE generates an STM32WB55 linker/memory map that places 
.MB_MEM2 in an SRAM2 region that bus-faults after the installed wireless stack reserves/protects SRAM2. A manually adjusted linker script placing MB_MEM1/.MB_MEM2 at 0x20038000 works.  

Observed: 

Generated/bad .MB_MEM2: 0x200301E4..0x20030A67

Edited/Working .MB_MEM2: 0x200381BC..0x20038A3F

 

The CubeMX-generated .ld file gives this fault:
HardFault before main()
CFSR = 0x00000400 = IMPRECISERR
Stacked PC = 0x080048CE, inside LoopCopyDataInit
R0/R1/R2 match .MB_MEM2 copy bounds

 

Attached .map .ld  .ioc

> 
STM32_Programmer_CLI.exe -c port=SWD freq=1000 mode=HOTPLUG -fusgetstate
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------

ST-LINK SN : X
ST-LINK FW : V2J47S7
Board : --
Voltage : 3.30V
SWD freq : 950 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev Y
Device name : STM32WB5x/35xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD5
Debug in Low Power mode enabled

 

> STM32_Programmer_CLI.exe -c port=SWD freq=1000 mode=HOTPLUG -fusopgetversion
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------

ST-LINK SN : X
ST-LINK FW : V2J47S7
Board : --
Voltage : 3.30V
SWD freq : 950 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev Y
Device name : STM32WB5x/35xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD5
Debug in Low Power mode enabled

FUS Operator Version : v1.f.b

 

> STM32_Programmer_CLI.exe -c port=SWD freq=1000 mode=HOTPLUG -ob displ
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------

ST-LINK SN : X
ST-LINK FW : V2J47S7
Board : --
Voltage : 3.30V
SWD freq : 950 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev Y
Device name : STM32WB5x/35xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD5
Debug in Low Power mode enabled


UPLOADING OPTION BYTES DATA ...

Bank : 0x00
Address : 0x58004020
Size : 96 Bytes

 

Bank : 0x01
Address : 0x58004080
Size : 8 Bytes


OPTION BYTES BANK: 0

Read Out Protection:

RDP : 0xAA (Level 0, no protection)

BOR Level:

BOR_LEV : 0x0 (BOR Level 0 reset level threshold is around 1.7 V)

User Configuration:

nBOOT0 : 0x1 (nBOOT0=1 Boot from main Flash)
nBOOT1 : 0x1 (Boot from code area if BOOT0=0 otherwise system Flash)
nSWBOOT0 : 0x0 (BOOT0 taken from the option bit nBOOT0)
SRAM2RST : 0x0 (SRAM2 erased when a system reset occurs)
SRAM2PE : 0x1 (SRAM2 parity check disable)
nRST_STOP : 0x1 (No reset generated when entering the Stop mode)
nRST_STDBY : 0x1 (No reset generated when entering the Standby mode)
nRSTSHDW : 0x1 (No reset generated when entering the Shutdown mode)
WWDGSW : 0x1 (Software window watchdog)
IWDGSTDBY : 0x1 (Independent watchdog counter running in Standby mode)
IWDGSTOP : 0x1 (Independent watchdog counter running in Stop mode)
IWDGSW : 0x1 (Software independent watchdog)
IPCCDBA : 0x0 (0x0)

Security Configuration Option bytes - 1:

ESE : 0x1 (Security enabled)

PCROP Protection:

PCROP1A_STRT : 0x1FF (0x80FF800)
PCROP1A_END : 0x0 (0x8000800)
PCROP_RDP : 0x1 (PCROP zone is erased when RDP is decreased)
PCROP1B_STRT : 0x1FF (0x80FF800)
PCROP1B_END : 0x0 (0x8000800)

Write Protection:

WRP1A_STRT : 0xFF (0x80FF000)
WRP1A_END : 0x0 (0x8000000)
WRP1B_STRT : 0xFF (0x80FF000)
WRP1B_END : 0x0 (0x8000000)
OPTION BYTES BANK: 1

Security Configuration Option bytes - 2:

SFSA : 0xC7 (0x80C7000)
FSD : 0x0 (System and Flash secure)
DDS : 0x1 (CPU2 debug access disabled)
C2OPT : 0x1 (SBRV will address Flash)
NBRSD : 0x0 (SRAM2b is secure)
SNBRSA : 0xA (0x2003A800)
BRSD : 0x0 (SRAM2a is secure)
SBRSA : 0x2 (0x20030800)
SBRV : 0x31C00 (0x20000000)




1 reply

Ghofrane GSOURI
ST Technical Moderator
May 12, 2026 7:09 AM UTC

Hello @DrMotor 

I'm currently checking this behavior. I will get back to you ASAP.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.