Skip to main content
GMula.1
Associate
November 4, 2020
Question

CubeMX STM32F302 USART LL DMA generated code missing LL_DMA_SetPeriphAddress & LL_USART_EnableDMAReq_TX

I have setup on cubeMX (STM32F302R8 Nucleo board) version 6.0.1 USART1 to use DMA on TX.

I use LL driver for usart.

The generated code is the following :

 /* USART1_TX Init */
 LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_4, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
 
 LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_4, LL_DMA_PRIORITY_HIGH);
 
 LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_4, LL_DMA_MODE_NORMAL);
 
 LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_4, LL_DMA_PERIPH_NOINCREMENT);
 
 LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_4, LL_DMA_MEMORY_INCREMENT);
 
 LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_4, LL_DMA_PDATAALIGN_BYTE);
 
 LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_4, LL_DMA_MDATAALIGN_BYTE);
 
 USART_InitStruct.BaudRate = 115200;
 USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
 USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
 USART_InitStruct.Parity = LL_USART_PARITY_NONE;
 USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
 USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
 USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
 LL_USART_Init(USART1, &USART_InitStruct);
 LL_USART_DisableIT_CTS(USART1);
 LL_USART_ConfigAsyncMode(USART1);
 
 LL_USART_Enable(USART1);

It' doesn't works out the the box, because the following fonction call are missing :

LL_DMA_SetPeriphAddress(DMA1, LL_DMA_CHANNEL_4,(uint32_t) &USART1->TDR);
 
LL_USART_EnableDMAReq_TX(USART1);

Moreover, adding user code section at the on on initialisation fonction would be nice, for exemple to enable some IT or have the posibility to fix otheir generated code error.

...

void MX_USART1_UART_Init(void)
{
 LL_USART_InitTypeDef USART_InitStruct = {0};
 
 LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* Peripheral clock enable */
 LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_USART1);
 
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
 /**USART1 GPIO Configuration
 PA9 ------> USART1_TX
 PA10 ------> USART1_RX
 */
 GPIO_InitStruct.Pin = LL_GPIO_PIN_9|LL_GPIO_PIN_10;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
 GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
 GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 GPIO_InitStruct.Alternate = LL_GPIO_AF_7;
 LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /* USART1 DMA Init */
 
 /* USART1_RX Init */
 LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_5, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
 
 LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_5, LL_DMA_PRIORITY_LOW);
 
 LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_5, LL_DMA_MODE_CIRCULAR);
 
 LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_5, LL_DMA_PERIPH_NOINCREMENT);
 
 LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_5, LL_DMA_MEMORY_INCREMENT);
 
 LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_5, LL_DMA_PDATAALIGN_BYTE);
 
 LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_5, LL_DMA_MDATAALIGN_BYTE);
 
 /* USART1_TX Init */
 LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_4, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
 
 LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_4, LL_DMA_PRIORITY_HIGH);
 
 LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_4, LL_DMA_MODE_NORMAL);
 
 LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_4, LL_DMA_PERIPH_NOINCREMENT);
 
 LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_4, LL_DMA_MEMORY_INCREMENT);
 
 LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_4, LL_DMA_PDATAALIGN_BYTE);
 
 LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_4, LL_DMA_MDATAALIGN_BYTE);
 
 USART_InitStruct.BaudRate = 115200;
 USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
 USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
 USART_InitStruct.Parity = LL_USART_PARITY_NONE;
 USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
 USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
 USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
 LL_USART_Init(USART1, &USART_InitStruct);
 LL_USART_DisableIT_CTS(USART1);
 LL_USART_ConfigAsyncMode(USART1);
 
/* USER CODE BEGIN 0 */
 LL_DMA_SetPeriphAddress(DMA1, LL_DMA_CHANNEL_4,(uint32_t) &USART1->TDR);
 LL_USART_EnableDMAReq_TX(USART1);
 LL_DMA_EnableIT_TC(DMA1,LL_DMA_CHANNEL_4);
 LL_DMA_EnableIT_TE(DMA1,LL_DMA_CHANNEL_4);
/* USER CODE END 0 */
 
 LL_USART_Enable(USART1);
 
}

Gabriel.

This topic has been closed for replies.

3 replies

Nesrine.JLASSI
Visitor II
November 11, 2020

Hi @GMula.1​ 

Thanks for your post. I have raised your feedback internally to be reviewed and treated accordingly to the priority. We will give you an update as soon as possible.

Thanks for your contribution!

Best regards,

Nesrine

Nesrine.JLASSI
Visitor II
November 29, 2020

Hi @GMula.1​ 

LL_DMA_SetPeriphAddress is set in HAL function HAL_DMA_Start, this function is not called when configuring DMA in HAL==> Therefore, this function cannot be expected to be made in LL.

For the function LL_USART_EnableDMAReq_TX(USART1); it is not managed so, it will not be generated.

For the second point " adding user code section at the on on initialisation fonction would be nice, for exemple to enable some IT or have the posibility to fix otheir generated code error." ==> Our development team is currently working to fix this in the coming release.

Thanks for your contribution!

Best regards,

Nesrine

GMula.1
GMula.1Author
Associate
November 30, 2020

Hello @Nesrine.JLASSI​ ,

I do not understand your answer about LL_DMA_SetPeriphAddress.

First, please note that LL_DMA_SetPeriphAddress is not generated even if i use the DMA in LL mode too :

static void MX_DMA_Init(void)
{
 
 /* Init with LL driver */
 /* DMA controller clock enable */
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
 
 /* DMA interrupt init */
 /* DMA1_Channel6_IRQn interrupt configuration */
 NVIC_SetPriority(DMA1_Channel6_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
 NVIC_EnableIRQ(DMA1_Channel6_IRQn);
 /* DMA1_Channel7_IRQn interrupt configuration */
 NVIC_SetPriority(DMA1_Channel7_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
 NVIC_EnableIRQ(DMA1_Channel7_IRQn);
 
}
static void MX_USART2_UART_Init(void)
{
 
 /* USER CODE BEGIN USART2_Init 0 */
 
 /* USER CODE END USART2_Init 0 */
 
 LL_USART_InitTypeDef USART_InitStruct = {0};
 
 LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* Peripheral clock enable */
 LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_USART2);
 
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
 /**USART2 GPIO Configuration
 PA2 ------> USART2_TX
 PA3 ------> USART2_RX
 */
 GPIO_InitStruct.Pin = USART_TX_Pin|USART_RX_Pin;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
 GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 GPIO_InitStruct.Alternate = LL_GPIO_AF_7;
 LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /* USART2 DMA Init */
 
 /* USART2_RX Init */
 LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_6, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
 
 LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_6, LL_DMA_PRIORITY_LOW);
 
 LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_6, LL_DMA_MODE_NORMAL);
 
 LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_6, LL_DMA_PERIPH_NOINCREMENT);
 
 LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_6, LL_DMA_MEMORY_INCREMENT);
 
 LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_6, LL_DMA_PDATAALIGN_BYTE);
 
 LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_6, LL_DMA_MDATAALIGN_BYTE);
 
 /* USART2_TX Init */
 LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_7, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
 
 LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_7, LL_DMA_PRIORITY_LOW);
 
 LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_7, LL_DMA_MODE_NORMAL);
 
 LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_7, LL_DMA_PERIPH_NOINCREMENT);
 
 LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_7, LL_DMA_MEMORY_INCREMENT);
 
 LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_7, LL_DMA_PDATAALIGN_BYTE);
 
 LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_7, LL_DMA_MDATAALIGN_BYTE);
 
 /* USER CODE BEGIN USART2_Init 1 */
 
 /* USER CODE END USART2_Init 1 */
 USART_InitStruct.BaudRate = 38400;
 USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
 USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
 USART_InitStruct.Parity = LL_USART_PARITY_NONE;
 USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
 USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
 USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
 LL_USART_Init(USART2, &USART_InitStruct);
 LL_USART_DisableIT_CTS(USART2);
 LL_USART_ConfigAsyncMode(USART2);
 LL_USART_Enable(USART2);
 /* USER CODE BEGIN USART2_Init 2 */
 
 /* USER CODE END USART2_Init 2 */
 
}

Second :

The code generator setup almost every part of the DMA during initialisation of the UART ( Direction, channel, transfert mode/Size, Inc mode)

exept the peripheral address ???

what is the point here ?

Third : As user point of view, the code should work out of the box, or at least warn user about missing "setup" step.

with best regards,

Gabriel