Skip to main content
alex_embedded
Associate III
Sep 12, 2018 4:58 AM UTC
Question

CubeMX STM32F2 setting up ADC Bug

Hi All,

I am trying to set up an ADC channel on a specific pin on the STM32F207ZETx; PA0 (pin 34) and I have come across a pretty "big" problem.

When I set the pin and go to configure the pin, the "ADC1" button does not respond to a click and doesn't "look" like it usually does. I have attempted this on different STM32F2 MCUs with the same result. Everything seems fine with the F1 and F3 chips when I set them up.

0690X000006C0sZQAS.png

There is no icon, so to speak, on the button and nothing happens when I click it. To make things worse, once a project is saved like this it cannot be re-opened - it becomes corrupt.

I am using version 4.26.1

For reference this is what it is supposed to look like when there are no issues:

0690X000006C0seQAC.png

I wasn't sure where to post this, so if it is in the wrong thread I apologise in advance, any solutions would be greatly appreciated!

This topic has been closed for replies.

8 replies

Khouloud GARSI
ST Employee
Sep 12, 2018 5:44 PM UTC

Dear @alex_embedded​ ,

Many thanks for your feedback! This is the convenient place to report any potential bug you encounter.

I have reproduced the issue you're seeing and I will highlight it internally for further investigation.

We will answer you ASAP.

Thanks!

Khouloud.

Khouloud GARSI
ST Employee
Sep 12, 2018 5:48 PM UTC

Hi @alex_embedded​ ,

Just note that the new release of the STM32CubeMX tool (V4.27.0) is now available under ST website.

Link:

https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-configurators-and-code-generators/stm32cubemx.html

Khouloud.

Tesla DeLorean
Guru
Sep 12, 2018 5:53 PM UTC

FYI CubeMX 4.26.1 is NOT recognizing that an update is available, server side database might need updating.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Khouloud GARSI
ST Employee
Sep 12, 2018 5:56 PM UTC

Thanks @Community member​  for bringing this to our attention.

I will report this to our teams immediately.

Khouloud.

alex_embedded
Associate III
Sep 13, 2018 2:38 AM UTC

Hi All,

Just a quick update,

CubeMX did not find the new version but I did download it and install it manually. My project has been migrated to the new version and I can confirm that the ADC setup appears to be working!

I have no tried to save yet, but I assume it'll save without any troubles. If not I'll let you all know!

Thanks for the help!

Khouloud GARSI
ST Employee
Sep 13, 2018 8:04 AM UTC

Thanks for the update. If you have any feedback, do not hesitate to share it here ;)

Khouloud.

Tesla DeLorean
Guru
Sep 17, 2018 4:08 PM UTC

@Khouloud GARSI​ database looks to have been updated over weekend, 4.26.1 has recognized availability of update. Thanks

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Khouloud GARSI
ST Employee
Sep 17, 2018 4:12 PM UTC

You're always welcome Clive!