Skip to main content
craig2
Visitor II
Mar 12, 2014 9:17 PM UTC
Question

CubeMX Selecting timer Enocder Interface.

Posted on March 12, 2014 at 22:17

I am trying to use the STM32CubeMX tool to select and generate initialization code for the encoder interface.  I am using the Discovery board (STM32F407VGT) and trying to configure timer 5, but not sure how to get it to allow me to select this interface.  It is grayed out and not sure how to resolve it.  Anyone been able to do this?  Also there does not seem to be an motor encoder example using the new HAL layer,  if any one can point me to one, to would be helpful.  

Thanks

#motor-encoder #st32cubemx
This topic has been closed for replies.

2 replies

stm32cube-t
ST Employee
Mar 13, 2014 9:26 AM UTC
Posted on March 13, 2014 at 10:26

Leave the mouse some seconds over the grayed out field: a tooltip is displayed indicating the fields that need to be configured so that  the grayed out field becomes active.

StephaneF
ST Technical Moderator
Mar 13, 2014 10:36 AM UTC
Posted on March 13, 2014 at 11:36

hello,

In your specific case , as the encoder uses CH1 and CH2 inputs ,you should let both TIM5 Channel 1 and Channel 2 as ''Disabled'' and use another channel for the input capture fonction you would need.

regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.