Skip to main content
JulienD
Associate III
Dec 11, 2018 8:26 AM UTC
Question

CubeMX pops up some dialog while in command line mode

Hello,

I'm using CubeMx in command line mode which is a VERY usefull feature.

I'm using it through a continuous integration system.

My concern is that CubeMx sometimes generates dialog box for "migrate" or "unavaible lib".

Because the process is running under another user session or simply a distant server, the dialog does not appear and the process never ends. And more, there's nothing in the log file telling why.

I think that CubeMx should follow the standards when running in command line mode : It should never show any dialog box, fail is something is wrong and give a clue about what's wrong.

For today, I'm unable to imagine what is happening. The process stops after:

2018-12-11 17:21:07,870 [INFO] ThirdPartyDb:263 - Close Third Party DataBase File (C:/Windows/system32/config/systemprofile/.stm32cubemx/plugins/thirdparty/db/thirdparties_db.xml)
2018-12-11 17:21:07,877 [INFO] IntegrityCheckThread:94 - End integrity checks thread
2018-12-11 17:21:08,345 [INFO] ApiDbMcu:310 - Load IP Config File for FREERTOS
2018-12-11 17:21:08,588 [INFO] UtilMem:74 - Before build in PCC Used Memory: 188411384 Bytes (1581252608)
2018-12-11 17:21:08,775 [INFO] SharedServices:56 - Folder for power plug-in: C:/Windows/system32/config/systemprofile/.stm32cubemx/plugins/power
2018-12-11 17:21:08,775 [INFO] UtilMem:74 - After build in PCC Used Memory: 217346592 Bytes (1581252608)
2018-12-11 17:21:08,813 [INFO] OpenFileManager:275 - Restore cursor
2018-12-11 17:21:08,839 [INFO] DbMcusXml:106 - Load MCU database from C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\\db\/mcu/families.xml
2018-12-11 17:21:09,099 [INFO] DbMcusJson:86 - JSON generation date=Tue Jul 17 15:19:56 CEST 2018 (1531833596)
2018-12-11 17:21:09,695 [INFO] DbMcus:186 - Found 1207 MCUs (1165 are supported by CubeMX, 1165 are visible in CubeMX)
2018-12-11 17:21:09,696 [INFO] ApiDb:146 - User favorites file not found: C:\Windows\system32\config\systemprofile/.stm32cubemx/favorites.mcus.txt
2018-12-11 17:21:09,696 [INFO] DbMcus:197 - Set 0 / 0 favorites MCUs
OK
project generate

What does the program just after this log?

Thanks

Julien

This topic has been closed for replies.