Skip to main content
Associate
November 21, 2024
Question

CubeMX not regenerating/updating middleware files

Hello,

 

I am upgrading a software from an existing project for (f7 mcu). Software is generated by an old version of stm32CubeMX installed in 2018 (never updated) (firmware version V1.14.0 ), and is using some middlewares, like FATFS. However I noticed that on each code generation, the files of the middleware folder are not getting updated.

Theferore I would greatly appreciate any help to answer the following :

-Why are those files not getting updated ? Is there a parameter somewhere in CubeMX that handles an eventual activation of the middleware files generation ?

-I plan to bring the project on modern tools (up to date stm32cubeIDE), will I be able to choose if the middlewares get generated ? Will a 2018/2019 version of a file like ff.c still work in a more recent environment ?

 

Kind reguards,

 

PF.

This topic has been closed for replies.

9 replies

Ghofrane GSOURI
ST Technical Moderator
November 21, 2024

Hello @Pierre-François 

First let me thank you for posting.

Could you please share your IOC in order to push further the investigation.

I will be waiting for your feedback.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
November 21, 2024

Hello @Ghofrane GSOURI 

Thank you for your immediate reply.

I will not be able to share any file unfortunately. I can provide any specific parameter of the ioc file that you need me to check.

Sorry for this inconvenience

Ghofrane GSOURI
ST Technical Moderator
November 21, 2024

Hello @Pierre-François 

I would appreciate it if you could give me the version of CubeMX you mentioned that has been installed since 2018 (without any updates) (firmware version V1.14.0), and the version you desire to use now.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
November 21, 2024

Version used by the current project : 5.0.1 (Win10)
Version of stm32cubeIDE to be used : 1.13.2 (Win11)
Thank you

 

Edit: In stm32cubeIDE 1.13.2 the version of cubeMX used is  6.9.2.202309101412 if I may add

Ghofrane GSOURI
ST Technical Moderator
November 21, 2024

Hello @Pierre-François 

Migrating an IOC file from an older version of STM32CubeMX (5.0.1) to a newer version (6.9.2),across multiple major versions, especially with a gap as significant as 23 versions can indeed lead to configuration issues.

Before making any changes, ensure you have a backup of your original .ioc file. This will allow you to revert if necessary.

Since you encounter issues with direct migration, using an incremental approach can help mitigate the issue .Consider migrating first to an intermediate version from 5.0.1 to 5.4.0 , then from 5.4.0 to 6.0.0, before moving to 6.x versions, repeat this process for each major version (6.0.0 → 6.4.0 → 6.9.2).

Finally review all configurations carefully, as some settings may not translate correctly due to significant changes in the software architecture between versions.

BR,

Ghofrane

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
November 21, 2024

Thank you for your help on the migration, I will make sure to follow these steps.

About the more immediate problem of the middleware files, like FATFS, not getting updated with code generation, could you tell me more about it ? I would like to know if it's possible to toggle it somewhere in the MX settings. Depending on how the migration goes, it could not be a problem if they are spared from the generation but I would like to be sure I can control it.

Reguards,

 

PF