Skip to main content
RCapr.1
Visitor II
Aug 16, 2020 10:49 AM UTC
Question

CUBEMX not properly configuring window comparator in STM32L053

Using CUBEMX 6 to configure the two comparators in STM32L053 in window mode this initialization code is generated:

COMP_HandleTypeDef hcomp1;
COMP_HandleTypeDef hcomp2;
 
/* COMP1 init function */
void MX_COMP1_Init(void)
{
 
 hcomp1.Instance = COMP1;
 hcomp1.Init.InvertingInput = COMP_INPUT_MINUS_DAC1_CH1;
 hcomp1.Init.NonInvertingInput = COMP_INPUT_PLUS_IO1;
 hcomp1.Init.LPTIMConnection = COMP_LPTIMCONNECTION_DISABLED;
 hcomp1.Init.OutputPol = COMP_OUTPUTPOL_NONINVERTED;
 hcomp1.Init.Mode = COMP_POWERMODE_ULTRALOWPOWER;
 hcomp1.Init.WindowMode = COMP_WINDOWMODE_COMP1_INPUT_PLUS_COMMON;
 hcomp1.Init.TriggerMode = COMP_TRIGGERMODE_IT_FALLING;
 if (HAL_COMP_Init(&hcomp1) != HAL_OK)
 {
 Error_Handler();
 }
 
}
/* COMP2 init function */
void MX_COMP2_Init(void)
{
 
 hcomp2.Instance = COMP2;
 hcomp2.Init.InvertingInput = COMP_INPUT_MINUS_IO1;
 hcomp2.Init.NonInvertingInput = COMP_INPUT_PLUS_IO1;
 hcomp2.Init.LPTIMConnection = COMP_LPTIMCONNECTION_DISABLED;
 hcomp2.Init.OutputPol = COMP_OUTPUTPOL_NONINVERTED;
 hcomp2.Init.Mode = COMP_POWERMODE_ULTRALOWPOWER;
 hcomp2.Init.WindowMode = COMP_WINDOWMODE_DISABLE;
 hcomp2.Init.TriggerMode = COMP_TRIGGERMODE_IT_RISING;
 if (HAL_COMP_Init(&hcomp2) != HAL_OK)
 {
 Error_Handler();
 }
 
}

But this is not working, because the initial setting of window mode made in line 14:

hcomp1.Init.WindowMode = COMP_WINDOWMODE_COMP1_INPUT_PLUS_COMMON;

is cleared by the setting in line 32:

hcomp2.Init.WindowMode = COMP_WINDOWMODE_DISABLE;

To fix the bug I had to change the CUBEMX generated code, changing line 32 into:

hcomp2.Init.WindowMode = COMP_WINDOWMODE_COMP1_INPUT_PLUS_COMMON;

It seems a bug of the HAL libraries, because in STM32L053 there is not a window mode setting bit in the register COMP2_CSR.

An alternate, weaker, solution would be to exchange the order of the init sequence between the two comparators.

No other has had this issue?

This topic has been closed for replies.

1 reply

Nesrine.JLASSI
Visitor II
Oct 19, 2020 4:10 PM UTC

Hello @RCapr.1​ 

Could you please share your ioc file to check the issue.

Best regards,

Nesrine