CubeMX not linking files at all
- 4 replies
- 1401 views
Hello there :)
I create a project with TouchGFX 4.24.1, then import it to CubeIDE 1.16.1, which are both the current versions. Once i open the .ioc file, it says the file need to either be migrated to 6.12.1 or I can use the file as is, which seems to be 6.12.0. So there might be some missmatch between the current software releases.
Furthermore, and what really is my problem right now, is once I adjust any settings in cubeMX (USB_FS, ETH+LwIP), the files do get generated normally in the project directory, but are not included/linked in the project in cubeIDE at all.
For small things this does'nt matter that much, but e.g. for LwIP there is so much stuff to manually add...
Do I have something setup wrong, can this be adjusted, or is this i known bug with the newest release? I already did a clean reinstall of all STM-Programs.
Example .ioc file attached (i just did a quick enable of USB and lwip for testing).
Thanks!